Properties¶
Property | Description |
---|---|
EdgesHiddenByEdges | Returns or sets the staus of edges hidden by edges. |
Hiddenline | Returns or sets the status of hiddenline. |
HiddenlineColor | Returns or sets the color of hidden line. |
HiddenlineFont | Returns or sets the font type of hidden line. |
HiddenlineWidth | Returns or sets the width of hidden line or edges. |
IncludeModelCurves | Returns or sets the status of include model curves. |
InterferingSolids | Returns or sets the status of interfering solids. |
InterferingSolidsOption | Returns or sets the status of interfering solids. |
ReferenceEdgesOnly | Returns or sets the status of reference edges only. |
SelfHidden | Returns or sets the status of self hidden. |
SmallFeature | Returns or sets the small feature option. |
SmallFeaturesTolerance | Returns or sets the value of small features tolerance. |
Methods¶
Property Detail¶
IncludeModelCurves¶
-
HiddenLinesViewPreferences.
IncludeModelCurves
¶ Returns or sets the status of include model curves.
This allows the modeling curves in drawing views to participate in hidden line processing. Most useful where drawing are produced with wireframe curves or 2D sketch curves.
-------------------------------------
Getter Method
Signature
IncludeModelCurves()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeModelCurves(includeModelCurves)
Parameters: includeModelCurves (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
InterferingSolids¶
-
HiddenLinesViewPreferences.
InterferingSolids
¶ Returns or sets the status of interfering solids.
This allows the correct rendering of hidden lines in a drawing member view with interfering solids.
-------------------------------------
Getter Method
Signature
InterferingSolids()
Returns: Return type: bool New in version NX5.0.0.
Deprecated since version NX6.0.0: Use
Preferences.HiddenLinesViewPreferences.InterferingSolidsOption
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
InterferingSolids(interferingSolids)
Parameters: interferingSolids (bool) – New in version NX5.0.0.
Deprecated since version NX6.0.0: Use
Preferences.HiddenLinesViewPreferences.InterferingSolidsOption
instead.License requirements: drafting (“DRAFTING”)
InterferingSolidsOption¶
-
HiddenLinesViewPreferences.
InterferingSolidsOption
¶ Returns or sets the status of interfering solids.
This allows the correct rendering of hidden lines in a drawing member view with interfering solids.
-------------------------------------
Getter Method
Signature
InterferingSolidsOption()
Returns: Return type: NXOpen.Preferences.HiddenLineInterferingSolidsOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterferingSolidsOption(interferingSolids)
Parameters: interferingSolids ( NXOpen.Preferences.HiddenLineInterferingSolidsOption
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ReferenceEdgesOnly¶
-
HiddenLinesViewPreferences.
ReferenceEdgesOnly
¶ Returns or sets the status of reference edges only.
This controls the rendering of hidden edges with annotation. If True, only hidden edges referencing annotations are rendered. Hidden edges not referenced by annotation are not rendered.
-------------------------------------
Getter Method
Signature
ReferenceEdgesOnly()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceEdgesOnly(referenceEdgesOnly)
Parameters: referenceEdgesOnly (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
SmallFeature¶
-
HiddenLinesViewPreferences.
SmallFeature
¶ Returns or sets the small feature option.
This allows the simplification or removal of rendering of small features in large scale assembly drawings. Not all small features are considered for simplified rendering. Only if the boundary of a small feature lies completely within a face of the model is the small feature’s display modified.
-------------------------------------
Getter Method
Signature
SmallFeature()
Returns: Return type: NXOpen.Preferences.HiddenLineSmallFeatureOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmallFeature(smallFeature)
Parameters: smallFeature ( NXOpen.Preferences.HiddenLineSmallFeatureOption
) –New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
SmallFeaturesTolerance¶
-
HiddenLinesViewPreferences.
SmallFeaturesTolerance
¶ Returns or sets the value of small features tolerance.
-------------------------------------
Getter Method
Signature
SmallFeaturesTolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmallFeaturesTolerance(smallFeaturesTolerance)
Parameters: smallFeaturesTolerance (float) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)