BaseViewPreferences Class¶
-
class
NXOpen.Preferences.
BaseViewPreferences
¶ Bases:
object
Represents set of Base View Preferences applicable to drafting views.
These settings apply to any newly created base view.
To obtain an instance of this class use
Preferences.ViewPreferences.BaseView
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
SetFacetedRepresentation | The status of faceted representation, if True the clipping bounds are inherited, else the imported model view is placed on the drawing with an Automatic Rectangular Boundary |
SetInheritClippingBoundary | The status of inherit clipping boundary, if True the model view’s clipping boundary are inherited when model view is imported onto the drawing, else the imported model view is placed on the drawing with an Automatic Rectangular Boundary. |
SetTransferAnnotation | The status of transfer annotation controls whether or not annotations created in a model view are transferred to the drawing when a view is imported. |
Method Detail¶
SetFacetedRepresentation¶
-
BaseViewPreferences.
SetFacetedRepresentation
¶ The status of faceted representation, if True the clipping bounds are inherited, else the imported model view is placed on the drawing with an Automatic Rectangular Boundary
Signature
SetFacetedRepresentation(isFacetedRepresentation)
Parameters: isFacetedRepresentation (bool) – New in version NX5.0.0.
Deprecated since version NX8.5.1: Use
Preferences.GeneralViewPreferences.ViewRepresentation
instead.License requirements: drafting (“DRAFTING”)
SetInheritClippingBoundary¶
-
BaseViewPreferences.
SetInheritClippingBoundary
¶ The status of inherit clipping boundary, if True the model view’s clipping boundary are inherited when model view is imported onto the drawing, else the imported model view is placed on the drawing with an Automatic Rectangular Boundary.
Signature
SetInheritClippingBoundary(isInheritClippingBoundary)
Parameters: isInheritClippingBoundary (bool) – Inherit XY clipping boundaries of model New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
SetTransferAnnotation¶
-
BaseViewPreferences.
SetTransferAnnotation
¶ The status of transfer annotation controls whether or not annotations created in a model view are transferred to the drawing when a view is imported.
Signature
SetTransferAnnotation(isTransferAnnotation)
Parameters: isTransferAnnotation (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)