PlotBuilder Class¶
-
class
NXOpen.
PlotBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.PlotBuilder
.This class contains all information relating to plotting. The user must specify the sheets to be plotted by setting the appropriate fields through the
NXOpen.PlotSourceBuilder
. For each sheet selected, a temporary CGM file name must be supplied. Once the sheets are selected, the user must set the plotter and profile fields. If the plotter selected is an image file (JPEG, TIFF, EMF, CGM, or PNG), then a graphic filename must also be supplied for each sheet selected. The PlotBuilder class also handles all Banner data and Manufacturing data to be used during plotting. This class is created usingNXOpen.PlotManager
.To create a new instance of this class, use
NXOpen.PlotManager.CreatePlotBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BannerMessage | Returns or sets the banner message. |
CharacterSize | Returns or sets the character size of the banner. |
ClsfData | Returns or sets the option to plot clsf data. |
ColorsWidthsBuilder | Returns the Colors Widths builder. |
Copies | Returns or sets the number of copies to be plotted. |
DisplayBanner | Returns or sets the display banner. |
ImageResolution | Returns or sets the resolution of images created for plotting shaded views. |
JobName | Returns or sets the job name to be used for plotting. |
Justification | Returns or sets the justification of the banner text. |
PlotType | Returns or sets the type of plot. |
PlotterText | Returns or sets the plotter text. |
PrinterGroupText | Returns or sets the printer group text. |
ProfileText | Returns or sets the profile text. |
RasterImages | Returns or sets the raster images option. |
Rotation | Returns or sets the rotation of the banner. |
ShadedGeometry | Returns or sets the shaded geometry as wireframe option. |
SourceBuilder | Returns the Source builder. |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the plotting tolerance. |
Units | Returns or sets the units used to create the banner. |
XDisplay | Returns or sets the X coordinate of a banner. |
XOffset | Returns or sets the X coordinate offset of a banner. |
YDisplay | Returns or sets the Y coordinate of a banner. |
YOffset | Returns or sets the Y coordinate offset of a banner. |
Methods¶
Method | Description |
---|---|
AddToPlotLayout | Add Plot to Layout. |
AdvancedPlot | Initialize the SDI dialog. |
ClearPlotLayout | Clear Plot from Layout. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFilenames | Gets all the temporary CGM filenames to be plotted. |
GetGraphicFilenames | Gets all the Graphic filenames to be saved. |
GetObject | Returns the object currently being edited by this builder. |
SaveCgm | Saves the selected sheets as CGM files. |
SetFilenames | Sets all the temporary CGM filenames to be plotted. |
SetGraphicFilenames | Sets all the Graphic filenames to be saved. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PlotBuilderImageResolutionOption Enumeration | Specifies the plot image resolution |
PlotBuilderJustificationOption Enumeration | Specifies the justification of the banner |
PlotBuilderPlotTypes Enumeration | Specifies the type of plot |
PlotBuilderRotationOption Enumeration | Specifies the rotation of the banner |
PlotBuilderUnitsOption Enumeration | Specifies which units are associated to the dimensions |
PlotBuilderXdisplayOption Enumeration | Specifies the x-coordinate for the banner location |
PlotBuilderYdisplayOption Enumeration | Specifies the y-coordinate for the banner location |
Property Detail¶
BannerMessage¶
-
PlotBuilder.
BannerMessage
¶ Returns or sets the banner message.
This text field will be added to the banner if Display Banner is set to true.
-------------------------------------
Getter Method
Signature
BannerMessage()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BannerMessage(bannerMessage)
Parameters: bannerMessage (str) – New in version NX5.0.0.
License requirements: None.
CharacterSize¶
-
PlotBuilder.
CharacterSize
¶ Returns or sets the character size of the banner.
If Display Banner is true, the character size value will be used to determine the size of the banner text.
-------------------------------------
Getter Method
Signature
CharacterSize()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CharacterSize(characterSize)
Parameters: characterSize (float) – New in version NX5.0.0.
License requirements: None.
ClsfData¶
-
PlotBuilder.
ClsfData
¶ Returns or sets the option to plot clsf data.
If clsf data is true, the current clsf data will be included in the plot.
-------------------------------------
Getter Method
Signature
ClsfData()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClsfData(clsfData)
Parameters: clsfData (bool) – New in version NX5.0.0.
License requirements: None.
ColorsWidthsBuilder¶
-
PlotBuilder.
ColorsWidthsBuilder
¶ Returns the Colors Widths builder.
The Colors Widths builder contains all information relating to both colors and widths.
-------------------------------------
Getter Method
Signature
ColorsWidthsBuilder()
Returns: New ColorsWidthsBuilder object Return type: NXOpen.PlotColorsWidthsBuilder
New in version NX5.0.0.
License requirements: None.
Copies¶
-
PlotBuilder.
Copies
¶ Returns or sets the number of copies to be plotted.
-------------------------------------
Getter Method
Signature
Copies()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Copies(copies)
Parameters: copies (int) – New in version NX5.0.0.
License requirements: None.
DisplayBanner¶
-
PlotBuilder.
DisplayBanner
¶ Returns or sets the display banner.
If true, the specified banner options will be used in adding a banner to the plot. If false, no banner will be used to plot.
-------------------------------------
Getter Method
Signature
DisplayBanner()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayBanner(displayBanner)
Parameters: displayBanner (bool) – New in version NX5.0.0.
License requirements: None.
ImageResolution¶
-
PlotBuilder.
ImageResolution
¶ Returns or sets the resolution of images created for plotting shaded views.
-------------------------------------
Getter Method
Signature
ImageResolution()
Returns: Return type: NXOpen.PlotBuilderImageResolutionOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageResolution(imageResolution)
Parameters: imageResolution ( NXOpen.PlotBuilderImageResolutionOption
) –New in version NX5.0.0.
License requirements: None.
JobName¶
-
PlotBuilder.
JobName
¶ Returns or sets the job name to be used for plotting.
-------------------------------------
Getter Method
Signature
JobName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
JobName(jobName)
Parameters: jobName (str) – New in version NX5.0.0.
License requirements: None.
Justification¶
-
PlotBuilder.
Justification
¶ Returns or sets the justification of the banner text.
If Display Banner is true, the justification will be used to position the banner text. This can be set to Left Justify, Center Justify, or Right Justify.
-------------------------------------
Getter Method
Signature
Justification()
Returns: Return type: NXOpen.PlotBuilderJustificationOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Justification(justification)
Parameters: justification ( NXOpen.PlotBuilderJustificationOption
) –New in version NX5.0.0.
License requirements: None.
PlotType¶
-
PlotBuilder.
PlotType
¶ Returns or sets the type of plot.
This can be Standard or Plot Using a Layout.
-------------------------------------
Getter Method
Signature
PlotType()
Returns: Return type: NXOpen.PlotBuilderPlotTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlotType(plotType)
Parameters: plotType ( NXOpen.PlotBuilderPlotTypes
) –New in version NX5.0.0.
License requirements: None.
PlotterText¶
-
PlotBuilder.
PlotterText
¶ Returns or sets the plotter text.
The plotter field represents which plotter the user wishes to plot to, it can be an available printer or an image type (JPEG, CGM, TIFF, EMF, or PNG). If the plotter is a printer, then the appropriate printer group containing the chosen printer must also be set.
-------------------------------------
Getter Method
Signature
PlotterText()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlotterText(plotter)
Parameters: plotter (str) – New in version NX5.0.0.
License requirements: None.
PrinterGroupText¶
-
PlotBuilder.
PrinterGroupText
¶ Returns or sets the printer group text.
The printer group must be set if a printer is used as the plotter.
-------------------------------------
Getter Method
Signature
PrinterGroupText()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrinterGroupText(printerGroup)
Parameters: printerGroup (str) – New in version NX5.0.0.
License requirements: None.
ProfileText¶
-
PlotBuilder.
ProfileText
¶ Returns or sets the profile text.
The profile must be a valid SDI created profile associated with the current plotter.
-------------------------------------
Getter Method
Signature
ProfileText()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProfileText(profile)
Parameters: profile (str) – New in version NX5.0.0.
License requirements: None.
RasterImages¶
-
PlotBuilder.
RasterImages
¶ Returns or sets the raster images option.
This option determines whether or not raster images will be used when plotting.
-------------------------------------
Getter Method
Signature
RasterImages()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RasterImages(rasterImages)
Parameters: rasterImages (bool) – New in version NX5.0.0.
License requirements: None.
Rotation¶
-
PlotBuilder.
Rotation
¶ Returns or sets the rotation of the banner.
This can be set to 0, 90, 180, or 270 and will determine the rotation of the banner if Display Banner is true.
-------------------------------------
Getter Method
Signature
Rotation()
Returns: Return type: NXOpen.PlotBuilderRotationOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rotation(rotation)
Parameters: rotation ( NXOpen.PlotBuilderRotationOption
) –New in version NX5.0.0.
License requirements: None.
ShadedGeometry¶
-
PlotBuilder.
ShadedGeometry
¶ Returns or sets the shaded geometry as wireframe option.
If set to true, this option will show shaded objects as wireframes. The shaded objects will be represented as shaded if this option is set to false.
-------------------------------------
Getter Method
Signature
ShadedGeometry()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedGeometry(shadedGeometry)
Parameters: shadedGeometry (bool) – New in version NX5.0.0.
License requirements: None.
SourceBuilder¶
-
PlotBuilder.
SourceBuilder
¶ Returns the Source builder.
The Source builder contains all data involving the sheets to to be plotted.
-------------------------------------
Getter Method
Signature
SourceBuilder()
Returns: New SourceBuilder object Return type: NXOpen.PlotSourceBuilder
New in version NX5.0.0.
License requirements: None.
Tolerance¶
-
PlotBuilder.
Tolerance
¶ Returns or sets the plotting tolerance.
The tolerance is a unitless value that controls the accuracy or smoothness of plotted curve geometry. Values must be greater than or equal to 0.0001. Smaller values produce smoother curves.
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX5.0.0.
License requirements: None.
Units¶
-
PlotBuilder.
Units
¶ Returns or sets the units used to create the banner.
The units can be either English or Metric and they pertain to the X-offset, the Y-offset, and the character size when creating a banner.
-------------------------------------
Getter Method
Signature
Units()
Returns: Return type: NXOpen.PlotBuilderUnitsOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Units(units)
Parameters: units ( NXOpen.PlotBuilderUnitsOption
) –New in version NX5.0.0.
License requirements: None.
XDisplay¶
-
PlotBuilder.
XDisplay
¶ Returns or sets the X coordinate of a banner.
If Display Banner is true, the X and Y coordinates will determine where the banner will appear when plotting. This can be set to Left, Center, or Right.
-------------------------------------
Getter Method
Signature
XDisplay()
Returns: Return type: NXOpen.PlotBuilderXdisplayOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XDisplay(xDisplay)
Parameters: xDisplay ( NXOpen.PlotBuilderXdisplayOption
) –New in version NX5.0.0.
License requirements: None.
XOffset¶
-
PlotBuilder.
XOffset
¶ Returns or sets the X coordinate offset of a banner.
If Display Banner is true, the X offset will be used as the offset value in combination with the X coordinate to determine where the banner will appear when plotting.
-------------------------------------
Getter Method
Signature
XOffset()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XOffset(xOffset)
Parameters: xOffset (float) – New in version NX5.0.0.
License requirements: None.
YDisplay¶
-
PlotBuilder.
YDisplay
¶ Returns or sets the Y coordinate of a banner.
If Display Banner is true, the X and Y coordinates will determine where the banner will appear when plotting. This can be set to Bottom, Center, or Top.
-------------------------------------
Getter Method
Signature
YDisplay()
Returns: Return type: NXOpen.PlotBuilderYdisplayOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YDisplay(yDisplay)
Parameters: yDisplay ( NXOpen.PlotBuilderYdisplayOption
) –New in version NX5.0.0.
License requirements: None.
YOffset¶
-
PlotBuilder.
YOffset
¶ Returns or sets the Y coordinate offset of a banner.
If Display Banner is true, the Y offset will be used as the offset value in combination with the Y coordinate to determine where the banner will appear when plotting.
-------------------------------------
Getter Method
Signature
YOffset()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YOffset(yOffset)
Parameters: yOffset (float) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddToPlotLayout¶
-
PlotBuilder.
AddToPlotLayout
¶ Add Plot to Layout.
This routine adds a sheet to the plot layout.
Signature
AddToPlotLayout()
New in version NX5.0.0.
License requirements: None.
AdvancedPlot¶
-
PlotBuilder.
AdvancedPlot
¶ Initialize the SDI dialog.
Signature
AdvancedPlot()
New in version NX5.0.0.
License requirements: None.
ClearPlotLayout¶
-
PlotBuilder.
ClearPlotLayout
¶ Clear Plot from Layout.
This routine clears all sheets from the plot layout.
Signature
ClearPlotLayout()
New in version NX5.0.0.
License requirements: None.
GetFilenames¶
-
PlotBuilder.
GetFilenames
¶ Gets all the temporary CGM filenames to be plotted.
This list will contain the full path of the temporary CGM file to be used during plotting. This list must equal the number of sheets selected to plot and these files will be deleted after the plotting operation is finished.
Signature
GetFilenames()
Returns: Return type: list of str New in version NX5.0.0.
License requirements: None.
GetGraphicFilenames¶
-
PlotBuilder.
GetGraphicFilenames
¶ Gets all the Graphic filenames to be saved.
If the plotter selected is an image type (JPEG, CGM, TIFF, EMF, or PNG) then the graphic filenames text list will contain the full path of where these images will be saved to disk. This list must equal the number of sheets selected to plot.
Signature
GetGraphicFilenames()
Returns: Return type: list of str New in version NX5.0.0.
License requirements: None.
SaveCgm¶
-
PlotBuilder.
SaveCgm
¶ Saves the selected sheets as CGM files.
Signature
SaveCgm()
New in version NX5.0.0.
License requirements: None.
SetFilenames¶
-
PlotBuilder.
SetFilenames
¶ Sets all the temporary CGM filenames to be plotted.
This list will contain the full path of the temporary CGM file to be used during plotting. This list must equal the number of sheets selected to plot and the files will be deleted after the plotting operation is finished.
Signature
SetFilenames(filenames)
Parameters: filenames (list of str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
License requirements: None.
SetGraphicFilenames¶
-
PlotBuilder.
SetGraphicFilenames
¶ Sets all the Graphic filenames to be saved.
If the plotter selected is an image type (JPEG, CGM, TIFF, EMF, or PNG) then the graphic filenames text list will contain the full path of where these images will be saved to disk. This list must equal the number of sheets selected to plot.
Signature
SetGraphicFilenames(filenames)
Parameters: filenames (list of str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX5.0.0.
License requirements: None.
Validate¶
-
PlotBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.