PartReopenReport Class¶
-
class
NXOpen.
PartReopenReport
¶ Bases:
NXOpen.TransientObject
Contains information about a part and its components after it has been reopened.
Instances of this class are returned from the following reopen methods:
NXOpen.BasePart.Reopen
NXOpen.BasePart.ReopenAs
NXOpen.PartCollection.ReopenAll
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
CouldNotResetWorkPart | Returns whether or not the work part failed to reset during the reopen operation. |
NumberReopenParts | Returns the number of parts that reopen was attempted on. |
WasDisplayPartReopened | Returns whether or not the display part was reopened by the reopen operation. |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetStatuses | Returns a list of objects representing information about the parts that were reopened during the reopen operation. |
Property Detail¶
CouldNotResetWorkPart¶
-
PartReopenReport.
CouldNotResetWorkPart
¶ Returns whether or not the work part failed to reset during the reopen operation.
-------------------------------------
Getter Method
Signature
CouldNotResetWorkPart()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
NumberReopenParts¶
-
PartReopenReport.
NumberReopenParts
¶ Returns the number of parts that reopen was attempted on.
-------------------------------------
Getter Method
Signature
NumberReopenParts()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
WasDisplayPartReopened¶
-
PartReopenReport.
WasDisplayPartReopened
¶ Returns whether or not the display part was reopened by the reopen operation.
-------------------------------------
Getter Method
Signature
WasDisplayPartReopened()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
PartReopenReport.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetStatuses¶
-
PartReopenReport.
GetStatuses
¶ Returns a list of objects representing information about the parts that were reopened during the reopen operation.
Signature
GetStatuses()
Returns: Return type: list of NXOpen.PartReopenStatus
New in version NX6.0.1.
License requirements: None.