PartPartFamilyAttrType Enumeration¶
NXOpen.Part.PartFamilyAttrType is an alias for NXOpen.PartPartFamilyAttrType
-
class
NXOpen.
PartPartFamilyAttrType
¶ Bases:
object
The part family attribute types.
New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.PartFamily.FamilyAttributeAttrType
insteadEnum Members
Enum Member Enum Member Description TextType text attributeNumericType numeric attributeIntegerType integer attributeDoubleType double attributeStringType string attributePartType part attributeNameType name attributeInstanceType instance attributeExpressionType expression attributeMirrorType mirror attributeDensityType density attributeFeatureType feature attribute-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-