PartDelayedUpdateStatusDelayStatusInfo_Struct Struct¶
NXOpen.PartDelayedUpdateStatus.DelayStatusInfo is an alias for NXOpen.PartDelayedUpdateStatusDelayStatusInfo_Struct
-
class
NXOpen.
PartDelayedUpdateStatusDelayStatusInfo_Struct
¶ Bases:
object
Logical structure of part delayed update status
Fields¶
Field | Description |
---|---|
SessionDelayed | The part is delayed because geometry and expressions are delayed. |
ExplicitDelayed | The part is frozen in this session. |
FrozenDelayed | The part is frozen for all sessions. |
NotDisplayedDelayed | The part is delayed because it’s not in the displayed assembly. |
DeferredDelayed | The part is deferred delayed. |
InternalDelayed | The part is internal delayed. |
ConstraintDelayed | The part is delayed because assembly constraints are delayed. |
SessionDelayed¶
-
PartDelayedUpdateStatusDelayStatusInfo_Struct.
SessionDelayed
¶ The part is delayed because geometry and expressions are delayed.
-------------------------------------
Getter Method Signature
SessionDelayed()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
SessionDelayed(value)
Parameters: value (bool) –
ExplicitDelayed¶
-
PartDelayedUpdateStatusDelayStatusInfo_Struct.
ExplicitDelayed
¶ The part is frozen in this session.
-------------------------------------
Getter Method Signature
ExplicitDelayed()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ExplicitDelayed(value)
Parameters: value (bool) –
FrozenDelayed¶
-
PartDelayedUpdateStatusDelayStatusInfo_Struct.
FrozenDelayed
¶ The part is frozen for all sessions.
-------------------------------------
Getter Method Signature
FrozenDelayed()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
FrozenDelayed(value)
Parameters: value (bool) –
NotDisplayedDelayed¶
-
PartDelayedUpdateStatusDelayStatusInfo_Struct.
NotDisplayedDelayed
¶ The part is delayed because it’s not in the displayed assembly.
-------------------------------------
Getter Method Signature
NotDisplayedDelayed()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
NotDisplayedDelayed(value)
Parameters: value (bool) –
DeferredDelayed¶
-
PartDelayedUpdateStatusDelayStatusInfo_Struct.
DeferredDelayed
¶ The part is deferred delayed.
-------------------------------------
Getter Method Signature
DeferredDelayed()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
DeferredDelayed(value)
Parameters: value (bool) –
InternalDelayed¶
-
PartDelayedUpdateStatusDelayStatusInfo_Struct.
InternalDelayed
¶ The part is internal delayed.
-------------------------------------
Getter Method Signature
InternalDelayed()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
InternalDelayed(value)
Parameters: value (bool) –
ConstraintDelayed¶
-
PartDelayedUpdateStatusDelayStatusInfo_Struct.
ConstraintDelayed
¶ The part is delayed because assembly constraints are delayed.
-------------------------------------
Getter Method Signature
ConstraintDelayed()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
ConstraintDelayed(value)
Parameters: value (bool) –