PartCloseResponses Class¶
-
class
NXOpen.
PartCloseResponses
¶ Bases:
NXOpen.TransientObject
Manages a list of part name/response pairs which are used to determine whether a part should be closed if modified during part close.
These responses are used as input into the following methods:
NXOpen.BasePart.Close
NXOpen.BasePart.Reopen
NXOpen.BasePart.ReopenAs
They are ignored in these methods unless
NXOpen.BasePartCloseModified
is set toNXOpen.BasePartCloseModified.UseResponses
.New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
AddResponse | Add a response to the list. |
Dispose | Free resources associated with the instance. |
Method Detail¶
AddResponse¶
-
PartCloseResponses.
AddResponse
¶ Add a response to the list.
Signature
AddResponse(partName, response)
Parameters: - partName (str) – Part with which to associate response NOTE: The full Unicode character set is not supported for this parameter.
- response (bool) – Whether or not to close the part if modified. A value of true means yes; a value of false means no.
New in version NX3.0.0.
License requirements: None.
Dispose¶
-
PartCloseResponses.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.