PartCleanup Class¶
-
class
NXOpen.
PartCleanup
¶ Bases:
NXOpen.TransientObject
Provides utilities to to eliminate certain inaccessible objects from the part file.
To use this utility, first create an instance of this class by calling
Session.NewPartCleanup
. Then, set any part cleanup actions that you wish to be performed by setting the appropriate properties on this class. By default, all the properties are set to “false” or “none”. Once all the properties are set, then call thePartCleanup.DoCleanup
method to actually perform the cleanup action.For more information on what the various part cleanup options do, see the Part Cleanup Options Dialog section of the Gateway Help.
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
CleanupAssemblyConstraints | Returns or sets the option that specifies whether to cleanup assembly constraints. |
CleanupCAMObjects | Returns or sets the option that specifies whether to delete or fix any corrupt internal CAM objects. |
CleanupDraftingObjects | Returns or sets the option that specifies whether to perform drafting cleanup. |
CleanupFeatureData | Returns or sets the option that specifies whether to perform solid cleanup. |
CleanupMatingData | Returns or sets the option that specifies whether to cleanup mating data. |
CleanupRoutingData | Returns or sets the option which determines if the routing part cleanup option should be performed. |
DeleteBrokenInterpartLinks | Returns or sets the option that specifies whether or not to delete all inter-part links where one or more components in that inter-part link have been removed. |
DeleteDuplicateLights | Returns or sets the option that specifies whether to delete duplicate light source objects from the part file. |
DeleteInvalidAttributes | Returns or sets the option that specifies whether to delete all invalid user attributes from the part file. |
DeleteMaterials | Returns or sets the option that specifies whether to delete all materials from the part file. |
DeleteSpreadSheetData | Returns or sets the option that specifies whether to delete all spreadsheets from the part file. |
DeleteUnusedExpressions | Returns or sets the option that specifies whether to delete expressions that are not used in the part. |
DeleteUnusedFonts | Returns or sets the option that specifies whether to remove character fonts that are not used in any drafting text in the current part. |
DeleteUnusedObjects | Returns or sets the option that specifies whether to delete all extraneous objects from the work part |
DeleteVisualEditorData | Returns or sets the option that specifies whether to delete Visual Editor data from the part file. |
FixOffplaneSketchCurves | Returns or sets the option that specifies whether to fix off-plane sketch curves. |
GroupsToDelete | Returns or sets the option that specifies what empty groups should be deleted. |
PartsToCleanup | Returns or sets the option that specifies what parts will be cleaned up when PartCleanup.DoCleanup is called. |
ResetComponentDisplay | Returns or sets the option that specifies whether to remove assembly-specific geometry in component parts. |
TurnOffHighlighting | Returns or sets the option that specifies whether to turn off highlighting for all displayable objects in the displayed part. |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
DoCleanup | Actually performs the part cleanup operation according to the properties set on this object |
Reset | Resets all the properties back to the default values (i. |
Enumerations¶
PartCleanupCleanupParts Enumeration | Which parts to clean up |
PartCleanupDeleteGroups Enumeration | Which empty groups to clean up |
PartCleanupResetComponentDisplayAction Enumeration | Assembly display clean up action |
Property Detail¶
CleanupAssemblyConstraints¶
-
PartCleanup.
CleanupAssemblyConstraints
¶ Returns or sets the option that specifies whether to cleanup assembly constraints.
-------------------------------------
Getter Method
Signature
CleanupAssemblyConstraints()
Returns: Return type: bool New in version NX7.5.5.
License requirements: None.
-------------------------------------
Setter Method
Signature
CleanupAssemblyConstraints(option)
Parameters: option (bool) – New in version NX7.5.5.
License requirements: None.
CleanupCAMObjects¶
-
PartCleanup.
CleanupCAMObjects
¶ Returns or sets the option that specifies whether to delete or fix any corrupt internal CAM objects.
-------------------------------------
Getter Method
Signature
CleanupCAMObjects()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CleanupCAMObjects(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
CleanupDraftingObjects¶
-
PartCleanup.
CleanupDraftingObjects
¶ Returns or sets the option that specifies whether to perform drafting cleanup.
-------------------------------------
Getter Method
Signature
CleanupDraftingObjects()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CleanupDraftingObjects(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
CleanupFeatureData¶
-
PartCleanup.
CleanupFeatureData
¶ Returns or sets the option that specifies whether to perform solid cleanup.
-------------------------------------
Getter Method
Signature
CleanupFeatureData()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CleanupFeatureData(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
CleanupMatingData¶
-
PartCleanup.
CleanupMatingData
¶ Returns or sets the option that specifies whether to cleanup mating data.
-------------------------------------
Getter Method
Signature
CleanupMatingData()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CleanupMatingData(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
CleanupRoutingData¶
-
PartCleanup.
CleanupRoutingData
¶ Returns or sets the option which determines if the routing part cleanup option should be performed.
-------------------------------------
Getter Method
Signature
CleanupRoutingData()
Returns: Return type: bool New in version NX7.5.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
CleanupRoutingData(option)
Parameters: option (bool) – New in version NX7.5.4.
License requirements: None.
DeleteBrokenInterpartLinks¶
-
PartCleanup.
DeleteBrokenInterpartLinks
¶ Returns or sets the option that specifies whether or not to delete all inter-part links where one or more components in that inter-part link have been removed.
-------------------------------------
Getter Method
Signature
DeleteBrokenInterpartLinks()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteBrokenInterpartLinks(option)
Parameters: option (bool) – New in version NX5.0.0.
License requirements: None.
DeleteDuplicateLights¶
-
PartCleanup.
DeleteDuplicateLights
¶ Returns or sets the option that specifies whether to delete duplicate light source objects from the part file.
-------------------------------------
Getter Method
Signature
DeleteDuplicateLights()
Returns: Return type: bool New in version NX7.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteDuplicateLights(option)
Parameters: option (bool) – New in version NX7.5.3.
License requirements: None.
DeleteInvalidAttributes¶
-
PartCleanup.
DeleteInvalidAttributes
¶ Returns or sets the option that specifies whether to delete all invalid user attributes from the part file.
-------------------------------------
Getter Method
Signature
DeleteInvalidAttributes()
Returns: Return type: bool New in version NX8.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteInvalidAttributes(option)
Parameters: option (bool) – New in version NX8.0.3.
License requirements: None.
DeleteMaterials¶
-
PartCleanup.
DeleteMaterials
¶ Returns or sets the option that specifies whether to delete all materials from the part file.
-------------------------------------
Getter Method
Signature
DeleteMaterials()
Returns: Return type: bool New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteMaterials(option)
Parameters: option (bool) – New in version NX7.5.2.
License requirements: None.
DeleteSpreadSheetData¶
-
PartCleanup.
DeleteSpreadSheetData
¶ Returns or sets the option that specifies whether to delete all spreadsheets from the part file.
-------------------------------------
Getter Method
Signature
DeleteSpreadSheetData()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteSpreadSheetData(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
DeleteUnusedExpressions¶
-
PartCleanup.
DeleteUnusedExpressions
¶ Returns or sets the option that specifies whether to delete expressions that are not used in the part.
-------------------------------------
Getter Method
Signature
DeleteUnusedExpressions()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteUnusedExpressions(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
DeleteUnusedFonts¶
-
PartCleanup.
DeleteUnusedFonts
¶ Returns or sets the option that specifies whether to remove character fonts that are not used in any drafting text in the current part.
-------------------------------------
Getter Method
Signature
DeleteUnusedFonts()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteUnusedFonts(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
DeleteUnusedObjects¶
-
PartCleanup.
DeleteUnusedObjects
¶ Returns or sets the option that specifies whether to delete all extraneous objects from the work part
-------------------------------------
Getter Method
Signature
DeleteUnusedObjects()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteUnusedObjects(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
DeleteVisualEditorData¶
-
PartCleanup.
DeleteVisualEditorData
¶ Returns or sets the option that specifies whether to delete Visual Editor data from the part file.
-------------------------------------
Getter Method
Signature
DeleteVisualEditorData()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteVisualEditorData(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
FixOffplaneSketchCurves¶
-
PartCleanup.
FixOffplaneSketchCurves
¶ Returns or sets the option that specifies whether to fix off-plane sketch curves.
-------------------------------------
Getter Method
Signature
FixOffplaneSketchCurves()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FixOffplaneSketchCurves(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
GroupsToDelete¶
-
PartCleanup.
GroupsToDelete
¶ Returns or sets the option that specifies what empty groups should be deleted.
-------------------------------------
Getter Method
Signature
GroupsToDelete()
Returns: Return type: NXOpen.PartCleanupDeleteGroups
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GroupsToDelete(option)
Parameters: option ( NXOpen.PartCleanupDeleteGroups
) –New in version NX3.0.0.
License requirements: None.
PartsToCleanup¶
-
PartCleanup.
PartsToCleanup
¶ Returns or sets the option that specifies what parts will be cleaned up when
PartCleanup.DoCleanup
is called.-------------------------------------
Getter Method
Signature
PartsToCleanup()
Returns: Return type: NXOpen.PartCleanupCleanupParts
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartsToCleanup(option)
Parameters: option ( NXOpen.PartCleanupCleanupParts
) –New in version NX3.0.0.
License requirements: None.
ResetComponentDisplay¶
-
PartCleanup.
ResetComponentDisplay
¶ Returns or sets the option that specifies whether to remove assembly-specific geometry in component parts.
-------------------------------------
Getter Method
Signature
ResetComponentDisplay()
Returns: Return type: NXOpen.PartCleanupResetComponentDisplayAction
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResetComponentDisplay(option)
Parameters: option ( NXOpen.PartCleanupResetComponentDisplayAction
) –New in version NX3.0.0.
License requirements: None.
TurnOffHighlighting¶
-
PartCleanup.
TurnOffHighlighting
¶ Returns or sets the option that specifies whether to turn off highlighting for all displayable objects in the displayed part.
-------------------------------------
Getter Method
Signature
TurnOffHighlighting()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TurnOffHighlighting(option)
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
PartCleanup.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.