NXObjectComputationalTime_Struct Struct¶
NXOpen.NXObject.ComputationalTime is an alias for NXOpen.NXObjectComputationalTime_Struct
-
class
NXOpen.
NXObjectComputationalTime_Struct
¶ Bases:
object
Holds the computational time value of a time attribute.
The time value held here is in the current time zone of the machine running the program. This is the same format as that used by the NX UFUN API to represent a time attribute value