NXMatrixCollection Class¶
-
class
NXOpen.
NXMatrixCollection
¶ Bases:
object
Represents a collection of NX Matrixes.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
Create | Creates an NXMatrix @return The new NXMatrix |
FindObject | Finds an NXMatrix with the given identifier as recorded in a journal @return |
Method Detail¶
Create¶
-
NXMatrixCollection.
Create
¶ Creates an NXMatrix
Signature
Create(element)
Parameters: element ( NXOpen.Matrix3x3
) – Orientation relative to the absolute coordinate system of the owning part. Must be orthonormal.MathUtils.Orthonormalize
can be used to make a matrix orthonormal.Returns: The new NXMatrix Return type: NXOpen.NXMatrix
New in version NX3.0.0.
License requirements: None.
FindObject¶
-
NXMatrixCollection.
FindObject
¶ Finds an NXMatrix with the given identifier as recorded in a journal
Signature
FindObject(sid)
Parameters: sid (str) – Journal identifier of the NXMatrix Returns: Return type: NXOpen.NXMatrix
New in version NX3.0.0.
License requirements: None.