PointOnCurveBuilder Class¶
-
class
NXOpen.Motion.
PointOnCurveBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a
NXOpen.Motion.PointOnCurveBuilder
To create a new instance of this class, use
NXOpen.Motion.PointOnCurveCollection.CreatePointOnCurveBuilder
Default values.
Property Value CurveParameterizedType Spacing New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CurveParameterizedType | Returns or sets the curve parameterized type |
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
Link | Returns the action link |
Name | Returns or sets the name |
Point | Returns or sets the selected point |
SpacingExpression | Returns the user defined spacing |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCurves | Returns the curves @return curve or edge |
GetObject | Returns the object currently being edited by this builder. |
SetCurves | Sets the curves |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CurveParameterizedType¶
-
PointOnCurveBuilder.
CurveParameterizedType
¶ Returns or sets the curve parameterized type
-------------------------------------
Getter Method
Signature
CurveParameterizedType()
Returns: Return type: NXOpen.Motion.CurveParameterizedTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveParameterizedType(curveParameterizedType)
Parameters: curveParameterizedType ( NXOpen.Motion.CurveParameterizedTypes
) –New in version NX8.0.0.
License requirements: mechanisms (“MECHANISMS”)
Link¶
-
PointOnCurveBuilder.
Link
¶ Returns the action link
-------------------------------------
Getter Method
Signature
Link()
Returns: Return type: NXOpen.Motion.SelectLink
New in version NX8.0.0.
License requirements: None.
Name¶
-
PointOnCurveBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Point¶
-
PointOnCurveBuilder.
Point
¶ Returns or sets the selected point
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
SpacingExpression¶
-
PointOnCurveBuilder.
SpacingExpression
¶ Returns the user defined spacing
-------------------------------------
Getter Method
Signature
SpacingExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Method Detail¶
GetCurves¶
-
PointOnCurveBuilder.
GetCurves
¶ Returns the curves
Signature
GetCurves()
Returns: curve or edge Return type: list of NXOpen.NXObject
New in version NX6.0.0.
License requirements: None.
SetCurves¶
-
PointOnCurveBuilder.
SetCurves
¶ Sets the curves
Signature
SetCurves(curves)
Parameters: curves (list of NXOpen.NXObject
) – curve or edgeNew in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Validate¶
-
PointOnCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.