MotionSolutionCollection Class¶
-
class
NXOpen.Motion.
MotionSolutionCollection
¶ Bases:
object
Represents a collection of Driver objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateSolutionBuilder | Creates an NXOpen.Motion.MotionSolutionBuilder . |
FindObject | Finds the NXOpen.Motion.MotionSolution object with the given name. |
GetActiveSolution | Get the active NXOpen.Motion.MotionSolution object of current session. |
SetActiveSolution | Set the active NXOpen.Motion.MotionSolution object of current session. |
Method Detail¶
CreateSolutionBuilder¶
-
MotionSolutionCollection.
CreateSolutionBuilder
¶ Creates an
NXOpen.Motion.MotionSolutionBuilder
.This class is used to construct an
NXOpen.Motion.MotionSolution
object.Signature
CreateSolutionBuilder(solution)
Parameters: solution ( NXOpen.Motion.MotionSolution
) – “NXOpen.Motion.MotionSolution
to be edited, if None then create a new oneReturns: Return type: NXOpen.Motion.MotionSolutionBuilder
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
MotionSolutionCollection.
FindObject
¶ Finds the
NXOpen.Motion.MotionSolution
object with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Name of the Solution object. Returns: NXOpen.Motion.MotionSolution
object with this name.Return type: NXOpen.Motion.MotionSolution
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetActiveSolution¶
-
MotionSolutionCollection.
GetActiveSolution
¶ Get the active
NXOpen.Motion.MotionSolution
object of current session.Signature
GetActiveSolution()
Returns: the active solution:py:class:NXOpen.Motion.MotionSolution Return type: NXOpen.Motion.MotionSolution
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetActiveSolution¶
-
MotionSolutionCollection.
SetActiveSolution
¶ Set the active
NXOpen.Motion.MotionSolution
object of current session.Signature
SetActiveSolution(activeSolution)
Parameters: activeSolution ( NXOpen.Motion.MotionSolution
) – the active solutionNXOpen.Motion.MotionSolution
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)