MotionSensorBuilder Class¶
-
class
NXOpen.Motion.
MotionSensorBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a
NXOpen.Motion.MotionSensorBuilder
To create a new instance of this class, use
NXOpen.Motion.MotionSensorCollection.CreateMotionSensorBuilder
Default values.
Property Value ComponentType LinearMagnitude ReferenceFrame Absolute Type Displacement New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ComponentType | Returns or sets the component type |
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
MeasurementObject | Returns the first marker object |
Name | Returns or sets the name |
ReferenceFrame | Returns or sets the reference frame type |
ReferenceMarker | Returns the reference marker object |
RelativeMarker | Returns the second marker object |
Tag | Returns the Tag for this object. |
Type | Returns or sets the sensor type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MotionSensorBuilderComponent Enumeration | component enumeration type |
MotionSensorBuilderReference Enumeration | reference frame enumeration type |
MotionSensorBuilderTypes Enumeration | sensor type |
Property Detail¶
ComponentType¶
-
MotionSensorBuilder.
ComponentType
¶ Returns or sets the component type
-------------------------------------
Getter Method
Signature
ComponentType()
Returns: Return type: NXOpen.Motion.MotionSensorBuilderComponent
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ComponentType(componentType)
Parameters: componentType ( NXOpen.Motion.MotionSensorBuilderComponent
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
MeasurementObject¶
-
MotionSensorBuilder.
MeasurementObject
¶ Returns the first marker object
-------------------------------------
Getter Method
Signature
MeasurementObject()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
Name¶
-
MotionSensorBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
ReferenceFrame¶
-
MotionSensorBuilder.
ReferenceFrame
¶ Returns or sets the reference frame type
-------------------------------------
Getter Method
Signature
ReferenceFrame()
Returns: Return type: NXOpen.Motion.MotionSensorBuilderReference
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceFrame(referenceFrame)
Parameters: referenceFrame ( NXOpen.Motion.MotionSensorBuilderReference
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
ReferenceMarker¶
-
MotionSensorBuilder.
ReferenceMarker
¶ Returns the reference marker object
-------------------------------------
Getter Method
Signature
ReferenceMarker()
Returns: Return type: NXOpen.Motion.SelectMarker
New in version NX6.0.0.
License requirements: None.
RelativeMarker¶
-
MotionSensorBuilder.
RelativeMarker
¶ Returns the second marker object
-------------------------------------
Getter Method
Signature
RelativeMarker()
Returns: Return type: NXOpen.Motion.SelectMarker
New in version NX6.0.0.
License requirements: None.
Type¶
-
MotionSensorBuilder.
Type
¶ Returns or sets the sensor type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Motion.MotionSensorBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Motion.MotionSensorBuilderTypes
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
MotionSensorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.