MotionEnvironment Class¶
-
class
NXOpen.Motion.
MotionEnvironment
¶ Bases:
object
Represents a Motion Environment
To obtain an instance of this class, refer to
NXOpen.Motion.MotionSession
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CheckCosimLicense | Checks the co-simulation license |
CheckFlexbodyLicense | Checks the flexible body dynamic license |
CheckMotorLicense | Checks the motor license |
GetJointWizardStatus | Gets the on-off status of joint wizard @return |
GetSolver | Gets current Motion solver @return |
SetAnalysisType | Sets the the analysis type |
SetComponentBasedMechanism | Sets component based mechanism |
SetJointWizardStatus | Sets the on-off status of joint wizard |
SetSolver | Sets Motion solver |
Enumerations¶
MotionEnvironmentAnalysis Enumeration | Represents analysis type of current mechanisms |
MotionEnvironmentJointWizardStatus Enumeration | Represents the on-off status of joint wizard |
MotionEnvironmentSolver Enumeration | Represents Motion solver of current mechanism |
Method Detail¶
CheckCosimLicense¶
-
MotionEnvironment.
CheckCosimLicense
¶ Checks the co-simulation license
Signature
CheckCosimLicense(checkCosimLicense)
Parameters: checkCosimLicense (bool) – Checks out or checks in co-simulation license New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
CheckFlexbodyLicense¶
-
MotionEnvironment.
CheckFlexbodyLicense
¶ Checks the flexible body dynamic license
Signature
CheckFlexbodyLicense(checkFlexbodyLicense)
Parameters: checkFlexbodyLicense (bool) – Checks out or checks in flexible body dynamic license New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
CheckMotorLicense¶
-
MotionEnvironment.
CheckMotorLicense
¶ Checks the motor license
Signature
CheckMotorLicense(checkMotorLicense)
Parameters: checkMotorLicense (bool) – Checks out or checks in motor license New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
GetJointWizardStatus¶
-
MotionEnvironment.
GetJointWizardStatus
¶ Gets the on-off status of joint wizard
Signature
GetJointWizardStatus()
Returns: Return type: NXOpen.Motion.MotionEnvironmentJointWizardStatus
New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetSolver¶
-
MotionEnvironment.
GetSolver
¶ Gets current Motion solver
Signature
GetSolver()
Returns: Return type: NXOpen.Motion.MotionEnvironmentSolver
New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetAnalysisType¶
-
MotionEnvironment.
SetAnalysisType
¶ Sets the the analysis type
Signature
SetAnalysisType(analysisType)
Parameters: analysisType ( NXOpen.Motion.MotionEnvironmentAnalysis
) – The analysis typeNew in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
SetComponentBasedMechanism¶
-
MotionEnvironment.
SetComponentBasedMechanism
¶ Sets component based mechanism
Signature
SetComponentBasedMechanism(componentBasedMech)
Parameters: componentBasedMech (bool) – Sets component based mechanism New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
SetJointWizardStatus¶
-
MotionEnvironment.
SetJointWizardStatus
¶ Sets the on-off status of joint wizard
Signature
SetJointWizardStatus(setting)
Parameters: setting ( NXOpen.Motion.MotionEnvironmentJointWizardStatus
) –New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetSolver¶
-
MotionEnvironment.
SetSolver
¶ Sets Motion solver
Signature
SetSolver(solver)
Parameters: solver ( NXOpen.Motion.MotionEnvironmentSolver
) –New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)