LoadTransferControl Class¶
-
class
NXOpen.Motion.
LoadTransferControl
¶ Bases:
NXOpen.NXObject
Represents the
NXOpen.Motion.LoadTransferControl
No support for KF
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AnimationStepBackward | Moves animation one step backward |
AnimationStepForward | Moves animation one step forward |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
ExportToSpreadsheet | Exports load transfer details to spreadsheet |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
Finish | Closes the load transfer control |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
PlayAnimation | Plays animation |
Prints a representation of this object to the system log file. | |
SetAnimationCurrentStep | Sets current step in animation |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetFlexibleLink | Sets flexible link |
SetLoadVectorScale | Sets load vector scale |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetRigidLink | Sets rigid link |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetViewPort | Sets view port |
StopAnimation | Stops animation |
UpdateFromSpreadsheet | Moves animation to cell position selected in spreadsheet |
Property Detail¶
IsOccurrence¶
-
LoadTransferControl.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
LoadTransferControl.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
LoadTransferControl.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
LoadTransferControl.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
LoadTransferControl.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
LoadTransferControl.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AnimationStepBackward¶
-
LoadTransferControl.
AnimationStepBackward
¶ Moves animation one step backward
Signature
AnimationStepBackward()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
AnimationStepForward¶
-
LoadTransferControl.
AnimationStepForward
¶ Moves animation one step forward
Signature
AnimationStepForward()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
ExportToSpreadsheet¶
-
LoadTransferControl.
ExportToSpreadsheet
¶ Exports load transfer details to spreadsheet
Signature
ExportToSpreadsheet()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
LoadTransferControl.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Finish¶
-
LoadTransferControl.
Finish
¶ Closes the load transfer control
Signature
Finish()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
PlayAnimation¶
-
LoadTransferControl.
PlayAnimation
¶ Plays animation
Signature
PlayAnimation()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
Print¶
-
LoadTransferControl.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetAnimationCurrentStep¶
-
LoadTransferControl.
SetAnimationCurrentStep
¶ Sets current step in animation
Signature
SetAnimationCurrentStep(step)
Parameters: step (int) – New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetFlexibleLink¶
-
LoadTransferControl.
SetFlexibleLink
¶ Sets flexible link
Signature
SetFlexibleLink(link)
Parameters: link ( NXOpen.Motion.FlexBody
) –New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetLoadVectorScale¶
-
LoadTransferControl.
SetLoadVectorScale
¶ Sets load vector scale
Signature
SetLoadVectorScale(scale, updateDisplay)
Parameters: - scale (float) –
- updateDisplay (bool) –
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetName¶
-
LoadTransferControl.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetRigidLink¶
-
LoadTransferControl.
SetRigidLink
¶ Sets rigid link
Signature
SetRigidLink(link)
Parameters: link ( NXOpen.Motion.Link
) –New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetViewPort¶
-
LoadTransferControl.
SetViewPort
¶ Sets view port
Signature
SetViewPort(viewPort)
Parameters: viewPort (int) – New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)