LinkBuilder Class¶
-
class
NXOpen.Motion.
LinkBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a
NXOpen.Motion.LinkBuilder
To create a new instance of this class, use
NXOpen.Motion.LinkCollection.CreateLinkBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DisplayScale | Returns or sets the icon display scale |
Fixed | Returns or sets the link fixed to the ground |
Geometries | Returns the geometries |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
InitialVelocity | Returns the initial velocity |
MassProperty | Returns the mass property |
Name | Returns or sets the name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Fixed¶
-
LinkBuilder.
Fixed
¶ Returns or sets the link fixed to the ground
-------------------------------------
Getter Method
Signature
Fixed()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Fixed(fixed)
Parameters: fixed (bool) – New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
Geometries¶
-
LinkBuilder.
Geometries
¶ Returns the geometries
-------------------------------------
Getter Method
Signature
Geometries()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX5.0.0.
License requirements: None.
InitialVelocity¶
-
LinkBuilder.
InitialVelocity
¶ Returns the initial velocity
-------------------------------------
Getter Method
Signature
InitialVelocity()
Returns: Return type: NXOpen.Motion.LinkInitialVelocity
New in version NX5.0.0.
License requirements: None.
MassProperty¶
-
LinkBuilder.
MassProperty
¶ Returns the mass property
-------------------------------------
Getter Method
Signature
MassProperty()
Returns: Return type: NXOpen.Motion.LinkMassProperty
New in version NX5.0.0.
License requirements: None.
Name¶
-
LinkBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
LinkBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.