GraphBuilderCurveData_Struct Struct¶
NXOpen.Motion.GraphBuilder.CurveData is an alias for NXOpen.Motion.GraphBuilderCurveData_Struct
-
class
NXOpen.Motion.
GraphBuilderCurveData_Struct
¶ Bases:
object
Contains the structure of curve associated with curve data.
Fields¶
Field | Description |
---|---|
MotionObject | Attribute object |
RequestIndex | Attribute request choice |
ComponentIndex | Attribute component choice |
RequestCsysIndex | Attribute csys choice |
MotionObject¶
-
GraphBuilderCurveData_Struct.
MotionObject
¶ Attribute object
-------------------------------------
Getter Method Signature
MotionObject()
Returns: Return type: NXOpen.NXObject
-------------------------------------
Setter Method
Signature
MotionObject(value)
Parameters: value ( NXOpen.NXObject
) –
RequestIndex¶
-
GraphBuilderCurveData_Struct.
RequestIndex
¶ Attribute request choice
-------------------------------------
Getter Method Signature
RequestIndex()
Returns: Return type: int -------------------------------------
Setter Method
Signature
RequestIndex(value)
Parameters: value (int) –
ComponentIndex¶
-
GraphBuilderCurveData_Struct.
ComponentIndex
¶ Attribute component choice
-------------------------------------
Getter Method Signature
ComponentIndex()
Returns: Return type: int -------------------------------------
Setter Method
Signature
ComponentIndex(value)
Parameters: value (int) –
RequestCsysIndex¶
-
GraphBuilderCurveData_Struct.
RequestCsysIndex
¶ Attribute csys choice
-------------------------------------
Getter Method Signature
RequestCsysIndex()
Returns: Return type: int -------------------------------------
Setter Method
Signature
RequestCsysIndex(value)
Parameters: value (int) –