CurveOnCurveBuilder Class¶
-
class
NXOpen.Motion.
CurveOnCurveBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a
NXOpen.Motion.CurveOnCurveBuilder
To create a new instance of this class, use
NXOpen.Motion.CurveOnCurveCollection.CreateCurveOnCurveBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
Name | Returns or sets the name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetICurve | Returns the first curves @return curve or edge |
GetJCurve | Returns the second curves @return curve or edge |
GetObject | Returns the object currently being edited by this builder. |
SetICurve | Sets the first curves |
SetJCurve | Sets second curves |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Name¶
-
CurveOnCurveBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
GetICurve¶
-
CurveOnCurveBuilder.
GetICurve
¶ Returns the first curves
Signature
GetICurve()
Returns: curve or edge Return type: list of NXOpen.NXObject
New in version NX6.0.0.
License requirements: None.
GetJCurve¶
-
CurveOnCurveBuilder.
GetJCurve
¶ Returns the second curves
Signature
GetJCurve()
Returns: curve or edge Return type: list of NXOpen.NXObject
New in version NX6.0.0.
License requirements: None.
SetICurve¶
-
CurveOnCurveBuilder.
SetICurve
¶ Sets the first curves
Signature
SetICurve(curves)
Parameters: curves (list of NXOpen.NXObject
) – curve or edgeNew in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetJCurve¶
-
CurveOnCurveBuilder.
SetJCurve
¶ Sets second curves
Signature
SetJCurve(curves)
Parameters: curves (list of NXOpen.NXObject
) – curve or edgeNew in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Validate¶
-
CurveOnCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.