CurveContactAdams Class¶
-
class
NXOpen.Motion.
CurveContactAdams
¶ Bases:
NXOpen.NXObject
Represents a
NXOpen.Motion.CurveContactAdams
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DynamicCoefficient | Returns or sets the dynamic coefficient |
DynamicCoefficientExpression | Returns the dynamic coefficient expression |
ForceExponent | Returns or sets the force exponent |
ForceExponentExpression | Returns the force exponent expression |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MaterialDamping | Returns or sets the material damping |
MaterialDampingExpression | Returns the material damping expression |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PenetrationDepth | Returns or sets the penetration depth |
PenetrationDepthExpression | Returns the penetration depth expression |
Prototype | Returns the prototype of this object if it is an occurrence. |
SlipVelocity | Returns or sets the slip velocity |
SlipVelocityExpression | Returns the slip velocity expression |
StaticCoefficient | Returns or sets the static coefficient |
StaticCoefficientExpression | Returns the static coefficient expression |
Stiffness | Returns or sets the stiffness |
StiffnessExpression | Returns the stiffness expression |
Tag | Returns the Tag for this object. |
TransitionVelocity | Returns or sets the transition velocity |
TransitionVelocityExpression | Returns the transition velocity expression |
Methods¶
Method | Description |
---|---|
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
DynamicCoefficient¶
-
CurveContactAdams.
DynamicCoefficient
¶ Returns or sets the dynamic coefficient
-------------------------------------
Getter Method
Signature
DynamicCoefficient()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.DynamicCoefficientExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
DynamicCoefficient(dynamicCoefficient)
Parameters: dynamicCoefficient (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.DynamicCoefficientExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
DynamicCoefficientExpression¶
-
CurveContactAdams.
DynamicCoefficientExpression
¶ Returns the dynamic coefficient expression
-------------------------------------
Getter Method
Signature
DynamicCoefficientExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ForceExponent¶
-
CurveContactAdams.
ForceExponent
¶ Returns or sets the force exponent
-------------------------------------
Getter Method
Signature
ForceExponent()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.ForceExponentExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
ForceExponent(forceExponent)
Parameters: forceExponent (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.ForceExponentExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
ForceExponentExpression¶
-
CurveContactAdams.
ForceExponentExpression
¶ Returns the force exponent expression
-------------------------------------
Getter Method
Signature
ForceExponentExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
IsOccurrence¶
-
CurveContactAdams.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
CurveContactAdams.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
MaterialDamping¶
-
CurveContactAdams.
MaterialDamping
¶ Returns or sets the material damping
-------------------------------------
Getter Method
Signature
MaterialDamping()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.MaterialDampingExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
MaterialDamping(materialDamping)
Parameters: materialDamping (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.MaterialDampingExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
MaterialDampingExpression¶
-
CurveContactAdams.
MaterialDampingExpression
¶ Returns the material damping expression
-------------------------------------
Getter Method
Signature
MaterialDampingExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Name¶
-
CurveContactAdams.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
CurveContactAdams.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
CurveContactAdams.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PenetrationDepth¶
-
CurveContactAdams.
PenetrationDepth
¶ Returns or sets the penetration depth
-------------------------------------
Getter Method
Signature
PenetrationDepth()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.PenetrationDepthExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
PenetrationDepth(penetrationDepth)
Parameters: penetrationDepth (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.PenetrationDepthExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
PenetrationDepthExpression¶
-
CurveContactAdams.
PenetrationDepthExpression
¶ Returns the penetration depth expression
-------------------------------------
Getter Method
Signature
PenetrationDepthExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Prototype¶
-
CurveContactAdams.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
SlipVelocity¶
-
CurveContactAdams.
SlipVelocity
¶ Returns or sets the slip velocity
-------------------------------------
Getter Method
Signature
SlipVelocity()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.SlipVelocityExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
SlipVelocity(slipVelocity)
Parameters: slipVelocity (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.SlipVelocityExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
SlipVelocityExpression¶
-
CurveContactAdams.
SlipVelocityExpression
¶ Returns the slip velocity expression
-------------------------------------
Getter Method
Signature
SlipVelocityExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
StaticCoefficient¶
-
CurveContactAdams.
StaticCoefficient
¶ Returns or sets the static coefficient
-------------------------------------
Getter Method
Signature
StaticCoefficient()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.StaticCoefficientExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
StaticCoefficient(staticCoefficient)
Parameters: staticCoefficient (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.StaticCoefficientExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
StaticCoefficientExpression¶
-
CurveContactAdams.
StaticCoefficientExpression
¶ Returns the static coefficient expression
-------------------------------------
Getter Method
Signature
StaticCoefficientExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Stiffness¶
-
CurveContactAdams.
Stiffness
¶ Returns or sets the stiffness
-------------------------------------
Getter Method
Signature
Stiffness()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.StiffnessExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
Stiffness(stiffness)
Parameters: stiffness (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.StiffnessExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
StiffnessExpression¶
-
CurveContactAdams.
StiffnessExpression
¶ Returns the stiffness expression
-------------------------------------
Getter Method
Signature
StiffnessExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
TransitionVelocity¶
-
CurveContactAdams.
TransitionVelocity
¶ Returns or sets the transition velocity
-------------------------------------
Getter Method
Signature
TransitionVelocity()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.TransitionVelocityExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
TransitionVelocity(transitionVelocity)
Parameters: transitionVelocity (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.CurveContactAdams.TransitionVelocityExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
TransitionVelocityExpression¶
-
CurveContactAdams.
TransitionVelocityExpression
¶ Returns the transition velocity expression
-------------------------------------
Getter Method
Signature
TransitionVelocityExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
CurveContactAdams.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
CurveContactAdams.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
CurveContactAdams.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.