BushingBuilder Class¶
-
class
NXOpen.Motion.
BushingBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a Motion BushingBuilder
To create a new instance of this class, use
NXOpen.Motion.BushingCollection.CreateBushingBuilder
Default values.
Property Value BushingCoefficients.CylindricalCoefficients.DampingCoefficients.Conical 0.0 BushingCoefficients.CylindricalCoefficients.DampingCoefficients.ConicalType Constant BushingCoefficients.CylindricalCoefficients.DampingCoefficients.Longitudinal 0.0 BushingCoefficients.CylindricalCoefficients.DampingCoefficients.Radial 0.0 BushingCoefficients.CylindricalCoefficients.DampingCoefficients.RadialType Constant BushingCoefficients.CylindricalCoefficients.DampingCoefficients.Torsional 0.0 BushingCoefficients.TorsionalCoefficients.DampingCoefficients.CoefficientsType Constant BushingCoefficients.TorsionalCoefficients.DampingCoefficients.XValue 0.0 BushingCoefficients.TorsionalCoefficients.DampingCoefficients.YValue 0.0 BushingCoefficients.TorsionalCoefficients.DampingCoefficients.ZValue 0.0 BushingDefine.OrientationType Vector New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BushingCoefficients | Returns the bushing coefficients |
BushingDefine | Returns the bushing define |
BushingType | Returns or sets the type |
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BushingBuilderBushingTypes Enumeration | Definitions of bushing type |
Property Detail¶
BushingCoefficients¶
-
BushingBuilder.
BushingCoefficients
¶ Returns the bushing coefficients
-------------------------------------
Getter Method
Signature
BushingCoefficients()
Returns: Return type: NXOpen.Motion.BushingCoefficients
New in version NX6.0.0.
License requirements: None.
BushingDefine¶
-
BushingBuilder.
BushingDefine
¶ Returns the bushing define
-------------------------------------
Getter Method
Signature
BushingDefine()
Returns: Return type: NXOpen.Motion.BushingDefine
New in version NX6.0.0.
License requirements: None.
BushingType¶
-
BushingBuilder.
BushingType
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
BushingType()
Returns: Return type: NXOpen.Motion.BushingBuilderBushingTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BushingType(type)
Parameters: type ( NXOpen.Motion.BushingBuilderBushingTypes
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
BushingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.