BodyContactRecurdyn Class¶
-
class
NXOpen.Motion.
BodyContactRecurdyn
¶ Bases:
NXOpen.NXObject
Represents a
NXOpen.Motion.BodyContactRecurdyn
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AutoGlobalMaxPenetrationFlag | Returns or sets the auto global maximum penetration flag |
AutoLocalMaxPenetrationFlag | Returns or sets the auto local maximum penetration flag |
BufferRadiusFactor | Returns or sets the Buffer Radius Factor |
BufferRadiusFactorExpression | Returns the Buffer Radius Factor expression |
ContactTypeOption | Returns or sets the contact type option |
CoulombFrictionOption | Returns or sets the coulomb friction option |
DynamicCoefficient | Returns or sets the dynamic coefficient |
DynamicCoefficientExpression | Returns the dynamic coefficient expression |
FirstGeometryBoundingBufferLength | Returns or sets the bounding Buffer Length |
FirstGeometryBoundingBufferLengthExpression | Returns the bounding Buffer Length expression |
FirstGeometryMaxFacetSizeFactor | Returns or sets the max Facet Size Factor |
FirstGeometryMaxFacetSizeFactorExpression | Returns the max Facet Size Factor expression |
FirstGeometryMaxFacetSizeFactorFlag | Returns or sets the max Facet Size Factor Flag |
FirstGeometryMaximumPenetration | Returns or sets the Plane Maximum Penetration of the first geometry |
FirstGeometryMaximumPenetrationExpression | Returns the Plane Maximum Penetration of the first geometry expresion |
FirstGeometryPlaneToleranceFactor | Returns or sets the Plane Tolerance Factor of the first geometry |
FirstGeometryPlaneToleranceFactorExpression | Returns the Plane Tolerance Factor of the first geometry expresion |
FirstGeometryPlaneToleranceFactorSolidContact | Returns or sets the Plane Tolerance Factor of the first geometry for solid contact |
FirstGeometryPlaneToleranceFactorSolidContactExpression | Returns the Plane Tolerance Factor of the first geometry for solid contact expression |
ForceExponent | Returns or sets the force exponent |
ForceExponentExpression | Returns the force exponent expression |
ForceModelType | Returns or sets the force model type |
FrictionVelocity | Returns or sets the friction velocity |
FrictionVelocityExpression | Returns the friction velocity expression |
GlobalMaxPenetration | Returns or sets the global Max. |
GlobalMaxPenetrationExpression | Returns the global Max. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
LocalMaxPenetration | Returns or sets the local Max. |
LocalMaxPenetrationExpression | Returns the local Max. |
MaterialDamping | Returns or sets the material damping |
MaterialDampingExpression | Returns the material damping expression |
MaximumStepSizeFactor | Returns or sets the Maximun Step Size Factor |
MaximumStepSizeFactorExpression | Returns the Maximun Step Size Factor expression |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PenetrationDepth | Returns or sets the penetration depth |
PenetrationDepthExpression | Returns the penetration depth expression |
Prototype | Returns the prototype of this object if it is an occurrence. |
ReboundDampingFactor | Returns or sets the rebound Damping Factor |
ReboundDampingFactorExpression | Returns the rebound Damping Factor expression |
ReboundDampingFactorFlag | Returns or sets the rebound Damping Factor Flag |
SecondGeometryBoundingBufferLength | Returns or sets the bounding Buffer Length |
SecondGeometryBoundingBufferLengthExpression | Returns the bounding Buffer Length expression |
SecondGeometryMaxFacetSizeFactor | Returns or sets the max Facet Size Factor |
SecondGeometryMaxFacetSizeFactorExpression | Returns the max Facet Size Factor expression |
SecondGeometryMaxFacetSizeFactorFlag | Returns or sets the max Facet Size Factor Flag |
SecondGeometryMaximumPenetration | Returns or sets the Plane Maximum Penetration of the second geometry |
SecondGeometryMaximumPenetrationExpression | Returns the Plane Maximum Penetration of the second geometry expression |
SecondGeometryPlaneToleranceFactor | Returns or sets the Plane Tolerance Factor of the second geometry |
SecondGeometryPlaneToleranceFactorExpression | Returns the Plane Tolerance Factor of the second geometry expression |
SecondGeometryPlaneToleranceFactorSolidContact | Returns or sets the Plane Tolerance Factor of the second geometry for solid contact |
SecondGeometryPlaneToleranceFactorSolidContactExpression | Returns the Plane Tolerance Factor of the second geometry for solid contact expression |
StaticCoefficient | Returns or sets the coulomb coefficient |
StaticCoefficientExpression | Returns the coulomb coefficient expression |
StictionVelocity | Returns or sets the stiction velocity |
StictionVelocityExpression | Returns the stiction velocity expression |
Stiffness | Returns or sets the stiffness |
StiffnessExpression | Returns the stiffness expression |
SurfaceTypeOption | Returns or sets the surface type option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
BodyContactRecurdynContactType Enumeration | the enum for contact type option of 3D contact |
BodyContactRecurdynCoulombFriction Enumeration | the enum for friction option of 3D contact |
BodyContactRecurdynForceModel Enumeration | the enum for forec model of 3D contact |
BodyContactRecurdynSurfaceType Enumeration | the enum for surface type option of 3D contact |
Property Detail¶
AutoGlobalMaxPenetrationFlag¶
-
BodyContactRecurdyn.
AutoGlobalMaxPenetrationFlag
¶ Returns or sets the auto global maximum penetration flag
-------------------------------------
Getter Method
Signature
AutoGlobalMaxPenetrationFlag()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoGlobalMaxPenetrationFlag(autoGlobalMaxPenetrationFlag)
Parameters: autoGlobalMaxPenetrationFlag (int) – New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
AutoLocalMaxPenetrationFlag¶
-
BodyContactRecurdyn.
AutoLocalMaxPenetrationFlag
¶ Returns or sets the auto local maximum penetration flag
-------------------------------------
Getter Method
Signature
AutoLocalMaxPenetrationFlag()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoLocalMaxPenetrationFlag(autoLocalMaxPenetrationFlag)
Parameters: autoLocalMaxPenetrationFlag (int) – New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
BufferRadiusFactor¶
-
BodyContactRecurdyn.
BufferRadiusFactor
¶ Returns or sets the Buffer Radius Factor
-------------------------------------
Getter Method
Signature
BufferRadiusFactor()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.BufferRadiusFactorExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
BufferRadiusFactor(bufferRadiusFactor)
Parameters: bufferRadiusFactor (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.BufferRadiusFactorExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
BufferRadiusFactorExpression¶
-
BodyContactRecurdyn.
BufferRadiusFactorExpression
¶ Returns the Buffer Radius Factor expression
-------------------------------------
Getter Method
Signature
BufferRadiusFactorExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ContactTypeOption¶
-
BodyContactRecurdyn.
ContactTypeOption
¶ Returns or sets the contact type option
-------------------------------------
Getter Method
Signature
ContactTypeOption()
Returns: Return type: NXOpen.Motion.BodyContactRecurdynContactType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContactTypeOption(contactType)
Parameters: contactType ( NXOpen.Motion.BodyContactRecurdynContactType
) –New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
CoulombFrictionOption¶
-
BodyContactRecurdyn.
CoulombFrictionOption
¶ Returns or sets the coulomb friction option
-------------------------------------
Getter Method
Signature
CoulombFrictionOption()
Returns: Return type: NXOpen.Motion.BodyContactRecurdynCoulombFriction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoulombFrictionOption(coulombFriction)
Parameters: coulombFriction ( NXOpen.Motion.BodyContactRecurdynCoulombFriction
) –New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
DynamicCoefficient¶
-
BodyContactRecurdyn.
DynamicCoefficient
¶ Returns or sets the dynamic coefficient
-------------------------------------
Getter Method
Signature
DynamicCoefficient()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.DynamicCoefficientExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
DynamicCoefficient(dynamicCoefficient)
Parameters: dynamicCoefficient (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.DynamicCoefficientExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
DynamicCoefficientExpression¶
-
BodyContactRecurdyn.
DynamicCoefficientExpression
¶ Returns the dynamic coefficient expression
-------------------------------------
Getter Method
Signature
DynamicCoefficientExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
FirstGeometryBoundingBufferLength¶
-
BodyContactRecurdyn.
FirstGeometryBoundingBufferLength
¶ Returns or sets the bounding Buffer Length
-------------------------------------
Getter Method
Signature
FirstGeometryBoundingBufferLength()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FirstGeometryBoundingBufferLengthExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
FirstGeometryBoundingBufferLength(boundingBufferLength)
Parameters: boundingBufferLength (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FirstGeometryBoundingBufferLengthExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
FirstGeometryBoundingBufferLengthExpression¶
-
BodyContactRecurdyn.
FirstGeometryBoundingBufferLengthExpression
¶ Returns the bounding Buffer Length expression
-------------------------------------
Getter Method
Signature
FirstGeometryBoundingBufferLengthExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
FirstGeometryMaxFacetSizeFactor¶
-
BodyContactRecurdyn.
FirstGeometryMaxFacetSizeFactor
¶ Returns or sets the max Facet Size Factor
-------------------------------------
Getter Method
Signature
FirstGeometryMaxFacetSizeFactor()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FirstGeometryMaxFacetSizeFactorExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
FirstGeometryMaxFacetSizeFactor(maxFacetSizeFactor)
Parameters: maxFacetSizeFactor (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FirstGeometryMaxFacetSizeFactorExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
FirstGeometryMaxFacetSizeFactorExpression¶
-
BodyContactRecurdyn.
FirstGeometryMaxFacetSizeFactorExpression
¶ Returns the max Facet Size Factor expression
-------------------------------------
Getter Method
Signature
FirstGeometryMaxFacetSizeFactorExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
FirstGeometryMaxFacetSizeFactorFlag¶
-
BodyContactRecurdyn.
FirstGeometryMaxFacetSizeFactorFlag
¶ Returns or sets the max Facet Size Factor Flag
-------------------------------------
Getter Method
Signature
FirstGeometryMaxFacetSizeFactorFlag()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstGeometryMaxFacetSizeFactorFlag(maxFacetSizeFactorFlag)
Parameters: maxFacetSizeFactorFlag (bool) – New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
FirstGeometryMaximumPenetration¶
-
BodyContactRecurdyn.
FirstGeometryMaximumPenetration
¶ Returns or sets the Plane Maximum Penetration of the first geometry
-------------------------------------
Getter Method
Signature
FirstGeometryMaximumPenetration()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FirstGeometryMaximumPenetrationExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
FirstGeometryMaximumPenetration(firstGeometryMaximumPenetration)
Parameters: firstGeometryMaximumPenetration (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FirstGeometryMaximumPenetrationExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
FirstGeometryMaximumPenetrationExpression¶
-
BodyContactRecurdyn.
FirstGeometryMaximumPenetrationExpression
¶ Returns the Plane Maximum Penetration of the first geometry expresion
-------------------------------------
Getter Method
Signature
FirstGeometryMaximumPenetrationExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
FirstGeometryPlaneToleranceFactor¶
-
BodyContactRecurdyn.
FirstGeometryPlaneToleranceFactor
¶ Returns or sets the Plane Tolerance Factor of the first geometry
-------------------------------------
Getter Method
Signature
FirstGeometryPlaneToleranceFactor()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FirstGeometryPlaneToleranceFactorExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
FirstGeometryPlaneToleranceFactor(firstGeometryPlaneToleranceFactor)
Parameters: firstGeometryPlaneToleranceFactor (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FirstGeometryPlaneToleranceFactorExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
FirstGeometryPlaneToleranceFactorExpression¶
-
BodyContactRecurdyn.
FirstGeometryPlaneToleranceFactorExpression
¶ Returns the Plane Tolerance Factor of the first geometry expresion
-------------------------------------
Getter Method
Signature
FirstGeometryPlaneToleranceFactorExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
FirstGeometryPlaneToleranceFactorSolidContact¶
-
BodyContactRecurdyn.
FirstGeometryPlaneToleranceFactorSolidContact
¶ Returns or sets the Plane Tolerance Factor of the first geometry for solid contact
-------------------------------------
Getter Method
Signature
FirstGeometryPlaneToleranceFactorSolidContact()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FirstGeometryPlaneToleranceFactorSolidContactExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
FirstGeometryPlaneToleranceFactorSolidContact(firstGeometryPlaneToleranceFactorSolidContact)
Parameters: firstGeometryPlaneToleranceFactorSolidContact (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FirstGeometryPlaneToleranceFactorSolidContactExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
FirstGeometryPlaneToleranceFactorSolidContactExpression¶
-
BodyContactRecurdyn.
FirstGeometryPlaneToleranceFactorSolidContactExpression
¶ Returns the Plane Tolerance Factor of the first geometry for solid contact expression
-------------------------------------
Getter Method
Signature
FirstGeometryPlaneToleranceFactorSolidContactExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ForceExponent¶
-
BodyContactRecurdyn.
ForceExponent
¶ Returns or sets the force exponent
-------------------------------------
Getter Method
Signature
ForceExponent()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.ForceExponentExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
ForceExponent(forceExponent)
Parameters: forceExponent (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.ForceExponentExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
ForceExponentExpression¶
-
BodyContactRecurdyn.
ForceExponentExpression
¶ Returns the force exponent expression
-------------------------------------
Getter Method
Signature
ForceExponentExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ForceModelType¶
-
BodyContactRecurdyn.
ForceModelType
¶ Returns or sets the force model type
-------------------------------------
Getter Method
Signature
ForceModelType()
Returns: Return type: NXOpen.Motion.BodyContactRecurdynForceModel
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForceModelType(forceModel)
Parameters: forceModel ( NXOpen.Motion.BodyContactRecurdynForceModel
) –New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
FrictionVelocity¶
-
BodyContactRecurdyn.
FrictionVelocity
¶ Returns or sets the friction velocity
-------------------------------------
Getter Method
Signature
FrictionVelocity()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FrictionVelocityExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
FrictionVelocity(frictionVelocity)
Parameters: frictionVelocity (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.FrictionVelocityExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
FrictionVelocityExpression¶
-
BodyContactRecurdyn.
FrictionVelocityExpression
¶ Returns the friction velocity expression
-------------------------------------
Getter Method
Signature
FrictionVelocityExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
GlobalMaxPenetration¶
-
BodyContactRecurdyn.
GlobalMaxPenetration
¶ Returns or sets the global Max.
Penetration
-------------------------------------
Getter Method
Signature
GlobalMaxPenetration()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.GlobalMaxPenetrationExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
GlobalMaxPenetration(globalMaxPenetration)
Parameters: globalMaxPenetration (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.GlobalMaxPenetrationExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
GlobalMaxPenetrationExpression¶
-
BodyContactRecurdyn.
GlobalMaxPenetrationExpression
¶ Returns the global Max.
Penetration expression
-------------------------------------
Getter Method
Signature
GlobalMaxPenetrationExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
IsOccurrence¶
-
BodyContactRecurdyn.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
BodyContactRecurdyn.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
LocalMaxPenetration¶
-
BodyContactRecurdyn.
LocalMaxPenetration
¶ Returns or sets the local Max.
Penetration
-------------------------------------
Getter Method
Signature
LocalMaxPenetration()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.LocalMaxPenetrationExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
LocalMaxPenetration(localMaxPenetration)
Parameters: localMaxPenetration (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.LocalMaxPenetrationExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
LocalMaxPenetrationExpression¶
-
BodyContactRecurdyn.
LocalMaxPenetrationExpression
¶ Returns the local Max.
Penetration expression
-------------------------------------
Getter Method
Signature
LocalMaxPenetrationExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
MaterialDamping¶
-
BodyContactRecurdyn.
MaterialDamping
¶ Returns or sets the material damping
-------------------------------------
Getter Method
Signature
MaterialDamping()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.MaterialDampingExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
MaterialDamping(materialDamping)
Parameters: materialDamping (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.MaterialDampingExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
MaterialDampingExpression¶
-
BodyContactRecurdyn.
MaterialDampingExpression
¶ Returns the material damping expression
-------------------------------------
Getter Method
Signature
MaterialDampingExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
MaximumStepSizeFactor¶
-
BodyContactRecurdyn.
MaximumStepSizeFactor
¶ Returns or sets the Maximun Step Size Factor
-------------------------------------
Getter Method
Signature
MaximumStepSizeFactor()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.MaximumStepSizeFactorExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumStepSizeFactor(maximumStepSizeFactor)
Parameters: maximumStepSizeFactor (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.MaximumStepSizeFactorExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
MaximumStepSizeFactorExpression¶
-
BodyContactRecurdyn.
MaximumStepSizeFactorExpression
¶ Returns the Maximun Step Size Factor expression
-------------------------------------
Getter Method
Signature
MaximumStepSizeFactorExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Name¶
-
BodyContactRecurdyn.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
BodyContactRecurdyn.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
BodyContactRecurdyn.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PenetrationDepth¶
-
BodyContactRecurdyn.
PenetrationDepth
¶ Returns or sets the penetration depth
-------------------------------------
Getter Method
Signature
PenetrationDepth()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.PenetrationDepthExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
PenetrationDepth(penetrationDepth)
Parameters: penetrationDepth (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.PenetrationDepthExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
PenetrationDepthExpression¶
-
BodyContactRecurdyn.
PenetrationDepthExpression
¶ Returns the penetration depth expression
-------------------------------------
Getter Method
Signature
PenetrationDepthExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Prototype¶
-
BodyContactRecurdyn.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
ReboundDampingFactor¶
-
BodyContactRecurdyn.
ReboundDampingFactor
¶ Returns or sets the rebound Damping Factor
-------------------------------------
Getter Method
Signature
ReboundDampingFactor()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.ReboundDampingFactorExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
ReboundDampingFactor(reboundDampingFactor)
Parameters: reboundDampingFactor (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.ReboundDampingFactorExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
ReboundDampingFactorExpression¶
-
BodyContactRecurdyn.
ReboundDampingFactorExpression
¶ Returns the rebound Damping Factor expression
-------------------------------------
Getter Method
Signature
ReboundDampingFactorExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ReboundDampingFactorFlag¶
-
BodyContactRecurdyn.
ReboundDampingFactorFlag
¶ Returns or sets the rebound Damping Factor Flag
-------------------------------------
Getter Method
Signature
ReboundDampingFactorFlag()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReboundDampingFactorFlag(reboundDampingFactorFlag)
Parameters: reboundDampingFactorFlag (bool) – New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
SecondGeometryBoundingBufferLength¶
-
BodyContactRecurdyn.
SecondGeometryBoundingBufferLength
¶ Returns or sets the bounding Buffer Length
-------------------------------------
Getter Method
Signature
SecondGeometryBoundingBufferLength()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.SecondGeometryBoundingBufferLengthExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
SecondGeometryBoundingBufferLength(boundingBufferLength)
Parameters: boundingBufferLength (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.SecondGeometryBoundingBufferLengthExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
SecondGeometryBoundingBufferLengthExpression¶
-
BodyContactRecurdyn.
SecondGeometryBoundingBufferLengthExpression
¶ Returns the bounding Buffer Length expression
-------------------------------------
Getter Method
Signature
SecondGeometryBoundingBufferLengthExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SecondGeometryMaxFacetSizeFactor¶
-
BodyContactRecurdyn.
SecondGeometryMaxFacetSizeFactor
¶ Returns or sets the max Facet Size Factor
-------------------------------------
Getter Method
Signature
SecondGeometryMaxFacetSizeFactor()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.SecondGeometryMaxFacetSizeFactorExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
SecondGeometryMaxFacetSizeFactor(maxFacetSizeFactor)
Parameters: maxFacetSizeFactor (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.SecondGeometryMaxFacetSizeFactorExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
SecondGeometryMaxFacetSizeFactorExpression¶
-
BodyContactRecurdyn.
SecondGeometryMaxFacetSizeFactorExpression
¶ Returns the max Facet Size Factor expression
-------------------------------------
Getter Method
Signature
SecondGeometryMaxFacetSizeFactorExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SecondGeometryMaxFacetSizeFactorFlag¶
-
BodyContactRecurdyn.
SecondGeometryMaxFacetSizeFactorFlag
¶ Returns or sets the max Facet Size Factor Flag
-------------------------------------
Getter Method
Signature
SecondGeometryMaxFacetSizeFactorFlag()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondGeometryMaxFacetSizeFactorFlag(maxFacetSizeFactorFlag)
Parameters: maxFacetSizeFactorFlag (bool) – New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
SecondGeometryMaximumPenetration¶
-
BodyContactRecurdyn.
SecondGeometryMaximumPenetration
¶ Returns or sets the Plane Maximum Penetration of the second geometry
-------------------------------------
Getter Method
Signature
SecondGeometryMaximumPenetration()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.SecondGeometryMaximumPenetration
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
SecondGeometryMaximumPenetration(secondGeometryMaximumPenetration)
Parameters: secondGeometryMaximumPenetration (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.SecondGeometryMaximumPenetration
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
SecondGeometryMaximumPenetrationExpression¶
-
BodyContactRecurdyn.
SecondGeometryMaximumPenetrationExpression
¶ Returns the Plane Maximum Penetration of the second geometry expression
-------------------------------------
Getter Method
Signature
SecondGeometryMaximumPenetrationExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SecondGeometryPlaneToleranceFactor¶
-
BodyContactRecurdyn.
SecondGeometryPlaneToleranceFactor
¶ Returns or sets the Plane Tolerance Factor of the second geometry
-------------------------------------
Getter Method
Signature
SecondGeometryPlaneToleranceFactor()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.SecondGeometryPlaneToleranceFactorExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
SecondGeometryPlaneToleranceFactor(secondGeometryPlaneToleranceFactor)
Parameters: secondGeometryPlaneToleranceFactor (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.SecondGeometryPlaneToleranceFactorExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
SecondGeometryPlaneToleranceFactorExpression¶
-
BodyContactRecurdyn.
SecondGeometryPlaneToleranceFactorExpression
¶ Returns the Plane Tolerance Factor of the second geometry expression
-------------------------------------
Getter Method
Signature
SecondGeometryPlaneToleranceFactorExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SecondGeometryPlaneToleranceFactorSolidContact¶
-
BodyContactRecurdyn.
SecondGeometryPlaneToleranceFactorSolidContact
¶ Returns or sets the Plane Tolerance Factor of the second geometry for solid contact
-------------------------------------
Getter Method
Signature
SecondGeometryPlaneToleranceFactorSolidContact()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.SecondGeometryPlaneToleranceFactorSolidContactExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
SecondGeometryPlaneToleranceFactorSolidContact(secondGeometryPlaneToleranceFactorSolidContact)
Parameters: secondGeometryPlaneToleranceFactorSolidContact (float) – New in version NX6.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.SecondGeometryPlaneToleranceFactorSolidContactExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
SecondGeometryPlaneToleranceFactorSolidContactExpression¶
-
BodyContactRecurdyn.
SecondGeometryPlaneToleranceFactorSolidContactExpression
¶ Returns the Plane Tolerance Factor of the second geometry for solid contact expression
-------------------------------------
Getter Method
Signature
SecondGeometryPlaneToleranceFactorSolidContactExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
StaticCoefficient¶
-
BodyContactRecurdyn.
StaticCoefficient
¶ Returns or sets the coulomb coefficient
-------------------------------------
Getter Method
Signature
StaticCoefficient()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.StaticCoefficientExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
StaticCoefficient(staticCoefficient)
Parameters: staticCoefficient (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.StaticCoefficientExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
StaticCoefficientExpression¶
-
BodyContactRecurdyn.
StaticCoefficientExpression
¶ Returns the coulomb coefficient expression
-------------------------------------
Getter Method
Signature
StaticCoefficientExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
StictionVelocity¶
-
BodyContactRecurdyn.
StictionVelocity
¶ Returns or sets the stiction velocity
-------------------------------------
Getter Method
Signature
StictionVelocity()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.StictionVelocityExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
StictionVelocity(stictionVelocity)
Parameters: stictionVelocity (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.StictionVelocityExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
StictionVelocityExpression¶
-
BodyContactRecurdyn.
StictionVelocityExpression
¶ Returns the stiction velocity expression
-------------------------------------
Getter Method
Signature
StictionVelocityExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Stiffness¶
-
BodyContactRecurdyn.
Stiffness
¶ Returns or sets the stiffness
-------------------------------------
Getter Method
Signature
Stiffness()
Returns: Return type: float New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.StiffnessExpression
to query or edit it.License requirements: None.
-------------------------------------
Setter Method
Signature
Stiffness(stiffness)
Parameters: stiffness (float) – New in version NX5.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.BodyContactRecurdyn.StiffnessExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
StiffnessExpression¶
-
BodyContactRecurdyn.
StiffnessExpression
¶ Returns the stiffness expression
-------------------------------------
Getter Method
Signature
StiffnessExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SurfaceTypeOption¶
-
BodyContactRecurdyn.
SurfaceTypeOption
¶ Returns or sets the surface type option
-------------------------------------
Getter Method
Signature
SurfaceTypeOption()
Returns: Return type: NXOpen.Motion.BodyContactRecurdynSurfaceType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceTypeOption(surfaceType)
Parameters: surfaceType ( NXOpen.Motion.BodyContactRecurdynSurfaceType
) –New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
FindObject¶
-
BodyContactRecurdyn.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
BodyContactRecurdyn.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
BodyContactRecurdyn.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.