BodyContactLms Class¶
-
class
NXOpen.Motion.
BodyContactLms
¶ Bases:
NXOpen.NXObject
Represents a
NXOpen.Motion.BodyContactLms
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ActionAngleTolerance | Returns the action angle tolerance |
ActionDistanceTolerance | Returns the action distance tolerance |
ActionEnableMaxFacetSize | Returns or sets the action enable max facet size |
ActionMaxFacetSize | Returns the action max facet size |
BaseAngleTolerance | Returns the base angle tolerance |
BaseDistanceTolerance | Returns the base distance tolerance |
BaseEnableMaxFacetSize | Returns or sets the base enable max facet size |
BaseMaxFacetSize | Returns the base max facet size |
CoulombFrictionOption | Returns or sets the coulomb friction option |
DynamicCoefficient | Returns the dynamic coefficient |
ForceExponent | Returns the force exponent |
FrictionVelocity | Returns the friction velocity |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MaterialDamping | Returns the material damping |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
StaticCoefficient | Returns the static coefficient |
StictionVelocity | Returns the stiction velocity |
Stiffness | Returns the stiffness |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
BodyContactLmsCoulombFriction Enumeration | the enum for friction option of 3D contact |
Property Detail¶
ActionAngleTolerance¶
-
BodyContactLms.
ActionAngleTolerance
¶ Returns the action angle tolerance
-------------------------------------
Getter Method
Signature
ActionAngleTolerance()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ActionDistanceTolerance¶
-
BodyContactLms.
ActionDistanceTolerance
¶ Returns the action distance tolerance
-------------------------------------
Getter Method
Signature
ActionDistanceTolerance()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ActionEnableMaxFacetSize¶
-
BodyContactLms.
ActionEnableMaxFacetSize
¶ Returns or sets the action enable max facet size
-------------------------------------
Getter Method
Signature
ActionEnableMaxFacetSize()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActionEnableMaxFacetSize(actionEnableMaxFacetSize)
Parameters: actionEnableMaxFacetSize (bool) – New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)
ActionMaxFacetSize¶
-
BodyContactLms.
ActionMaxFacetSize
¶ Returns the action max facet size
-------------------------------------
Getter Method
Signature
ActionMaxFacetSize()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
BaseAngleTolerance¶
-
BodyContactLms.
BaseAngleTolerance
¶ Returns the base angle tolerance
-------------------------------------
Getter Method
Signature
BaseAngleTolerance()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
BaseDistanceTolerance¶
-
BodyContactLms.
BaseDistanceTolerance
¶ Returns the base distance tolerance
-------------------------------------
Getter Method
Signature
BaseDistanceTolerance()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
BaseEnableMaxFacetSize¶
-
BodyContactLms.
BaseEnableMaxFacetSize
¶ Returns or sets the base enable max facet size
-------------------------------------
Getter Method
Signature
BaseEnableMaxFacetSize()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BaseEnableMaxFacetSize(baseEnableMaxFacetSize)
Parameters: baseEnableMaxFacetSize (bool) – New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)
BaseMaxFacetSize¶
-
BodyContactLms.
BaseMaxFacetSize
¶ Returns the base max facet size
-------------------------------------
Getter Method
Signature
BaseMaxFacetSize()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
CoulombFrictionOption¶
-
BodyContactLms.
CoulombFrictionOption
¶ Returns or sets the coulomb friction option
-------------------------------------
Getter Method
Signature
CoulombFrictionOption()
Returns: Return type: NXOpen.Motion.BodyContactLmsCoulombFriction
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoulombFrictionOption(coulombFrictionOption)
Parameters: coulombFrictionOption ( NXOpen.Motion.BodyContactLmsCoulombFriction
) –New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)
DynamicCoefficient¶
-
BodyContactLms.
DynamicCoefficient
¶ Returns the dynamic coefficient
-------------------------------------
Getter Method
Signature
DynamicCoefficient()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ForceExponent¶
-
BodyContactLms.
ForceExponent
¶ Returns the force exponent
-------------------------------------
Getter Method
Signature
ForceExponent()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
FrictionVelocity¶
-
BodyContactLms.
FrictionVelocity
¶ Returns the friction velocity
-------------------------------------
Getter Method
Signature
FrictionVelocity()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
IsOccurrence¶
-
BodyContactLms.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
BodyContactLms.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
MaterialDamping¶
-
BodyContactLms.
MaterialDamping
¶ Returns the material damping
-------------------------------------
Getter Method
Signature
MaterialDamping()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Name¶
-
BodyContactLms.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
BodyContactLms.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
BodyContactLms.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
BodyContactLms.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
StaticCoefficient¶
-
BodyContactLms.
StaticCoefficient
¶ Returns the static coefficient
-------------------------------------
Getter Method
Signature
StaticCoefficient()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
StictionVelocity¶
-
BodyContactLms.
StictionVelocity
¶ Returns the stiction velocity
-------------------------------------
Getter Method
Signature
StictionVelocity()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Stiffness¶
-
BodyContactLms.
Stiffness
¶ Returns the stiffness
-------------------------------------
Getter Method
Signature
Stiffness()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
BodyContactLms.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
BodyContactLms.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
BodyContactLms.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.