Properties¶
Property | Description |
---|---|
ButtonId | Returns the identifier of the button. |
ButtonName | Returns the name of the button. |
ButtonSensitivity | Returns or sets the sensitivity of the button. |
ButtonType | Returns the type of the button. |
ButtonTypeName | Returns the type name of the button. |
ToggleStatus | Returns or sets the toggle status of the button. |
Enumerations¶
MenuButtonSensitivityStatus Enumeration | Sensitivity Status |
MenuButtonToggle Enumeration | Toggle Status |
MenuButtonType Enumeration | Available button types |
Property Detail¶
ButtonId¶
-
MenuButton.
ButtonId
¶ Returns the identifier of the button.
-------------------------------------
Getter Method
Signature
ButtonId()
Returns: The identifier used for the button Return type: int New in version NX6.0.0.
License requirements: None.
ButtonName¶
-
MenuButton.
ButtonName
¶ Returns the name of the button.
-------------------------------------
Getter Method
Signature
ButtonName()
Returns: The name of the button Return type: str New in version NX6.0.0.
License requirements: None.
ButtonSensitivity¶
-
MenuButton.
ButtonSensitivity
¶ Returns or sets the sensitivity of the button.
-------------------------------------
Getter Method
Signature
ButtonSensitivity()
Returns: The sensitivity of the button Return type: NXOpen.MenuBar.MenuButtonSensitivityStatus
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ButtonSensitivity(sensitivity)
Parameters: sensitivity ( NXOpen.MenuBar.MenuButtonSensitivityStatus
) –New in version NX6.0.0.
License requirements: None.
ButtonType¶
-
MenuButton.
ButtonType
¶ Returns the type of the button.
-------------------------------------
Getter Method
Signature
ButtonType()
Returns: The type of the button Return type: NXOpen.MenuBar.MenuButtonType
New in version NX6.0.0.
License requirements: None.
ButtonTypeName¶
-
MenuButton.
ButtonTypeName
¶ Returns the type name of the button.
-------------------------------------
Getter Method
Signature
ButtonTypeName()
Returns: The type name of the button Return type: str New in version NX6.0.0.
License requirements: None.
ToggleStatus¶
-
MenuButton.
ToggleStatus
¶ Returns or sets the toggle status of the button.
-------------------------------------
Getter Method
Signature
ToggleStatus()
Returns: The toggle status of the button Return type: NXOpen.MenuBar.MenuButtonToggle
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToggleStatus(toggleStatus)
Parameters: toggleStatus ( NXOpen.MenuBar.MenuButtonToggle
) –New in version NX6.0.0.
License requirements: None.