VirtualAxisBuilder Class¶
-
class
NXOpen.Mechatronics.
VirtualAxisBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsJointBuilder
Represents a
NXOpen.Mechatronics.VirtualAxis
builderTo create a new instance of this class, use
NXOpen.Mechatronics.VirtualAxisCollection.CreateVirtualAxisBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AnchorPoint | Returns or sets the anchor point |
Attachment | Returns the attachment of joint. |
AxisType | Returns or sets the axis type |
Base | Returns the base of joint. |
Direction | Returns or sets the direction |
Name | Returns or sets the name. |
StartPosition | Returns the initial position of virtual axis |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAttachment | Sets the attachment. |
SetBase | Sets the base. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
VirtualAxisBuilderVirtualAxisType Enumeration | the Axis Type option. |
Property Detail¶
AnchorPoint¶
-
VirtualAxisBuilder.
AnchorPoint
¶ Returns or sets the anchor point
-------------------------------------
Getter Method
Signature
AnchorPoint()
Returns: Return type: NXOpen.Point
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AnchorPoint(point)
Parameters: point ( NXOpen.Point
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
AxisType¶
-
VirtualAxisBuilder.
AxisType
¶ Returns or sets the axis type
-------------------------------------
Getter Method
Signature
AxisType()
Returns: Return type: NXOpen.Mechatronics.VirtualAxisBuilderVirtualAxisType
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AxisType(axisType)
Parameters: axisType ( NXOpen.Mechatronics.VirtualAxisBuilderVirtualAxisType
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Direction¶
-
VirtualAxisBuilder.
Direction
¶ Returns or sets the direction
-------------------------------------
Getter Method
Signature
Direction()
Returns: Return type: NXOpen.Direction
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Direction(direction)
Parameters: direction ( NXOpen.Direction
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StartPosition¶
-
VirtualAxisBuilder.
StartPosition
¶ Returns the initial position of virtual axis
-------------------------------------
Getter Method
Signature
StartPosition()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
VirtualAxisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.