SlidingJointCollection Class¶
-
class
NXOpen.Mechatronics.
SlidingJointCollection
¶ Bases:
object
Represents a collection of Sliding Joint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateSlidingJointBuilder | Creates a NXOpen.Mechatronics.SlidingJointBuilder . |
FindObject | Finds the NXOpen.Mechatronics.SlidingJoint with the given name. |
Method Detail¶
CreateSlidingJointBuilder¶
-
SlidingJointCollection.
CreateSlidingJointBuilder
¶ Creates a
NXOpen.Mechatronics.SlidingJointBuilder
.Signature
CreateSlidingJointBuilder(slide)
Parameters: slide ( NXOpen.Mechatronics.SlidingJoint
) –NXOpen.Mechatronics.SlidingJoint
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.SlidingJointBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
SlidingJointCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.SlidingJoint
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.SlidingJoint
.Returns: NXOpen.Mechatronics.SlidingJoint
with this name.Return type: NXOpen.Mechatronics.SlidingJoint
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)