SignalAdapterBuilder Class¶
-
class
NXOpen.Mechatronics.
SignalAdapterBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.SignalAdapterBuilder
.To create a new instance of this class, use
NXOpen.Mechatronics.SignalAdapterCollection.CreateSignalAdapterBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
MaxSignalId | Returns or sets the maximum signal id. |
Name | Returns or sets the name. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetParameterData | Gets all parameter data. |
GetSignalData | Gets all signal data. |
SetParameterData | Sets all parameter data. |
SetSignalData | Sets all signal data. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SignalAdapterBuilderDataPortType Enumeration | Represents the data port type. |
SignalAdapterBuilderDataType Enumeration | Represents the data type. |
Structs¶
SignalAdapterBuilderParameterData_Struct Struct | Defines the parameter data. |
SignalAdapterBuilderSignalData_Struct Struct | Defines the signal data. |
Property Detail¶
MaxSignalId¶
-
SignalAdapterBuilder.
MaxSignalId
¶ Returns or sets the maximum signal id.
-------------------------------------
Getter Method
Signature
MaxSignalId()
Returns: Return type: int New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MaxSignalId(maxSignalId)
Parameters: maxSignalId (int) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Name¶
-
SignalAdapterBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetParameterData¶
-
SignalAdapterBuilder.
GetParameterData
¶ Gets all parameter data.
Signature
GetParameterData()
Returns: Array of parameter data Return type: list of NXOpen.Mechatronics.SignalAdapterBuilderParameterData_Struct
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetSignalData¶
-
SignalAdapterBuilder.
GetSignalData
¶ Gets all signal data.
Signature
GetSignalData()
Returns: Array of signal data Return type: list of NXOpen.Mechatronics.SignalAdapterBuilderSignalData_Struct
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetParameterData¶
-
SignalAdapterBuilder.
SetParameterData
¶ Sets all parameter data.
Signature
SetParameterData(parameterData)
Parameters: parameterData (list of NXOpen.Mechatronics.SignalAdapterBuilderParameterData_Struct
) – Array of parameter dataNew in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetSignalData¶
-
SignalAdapterBuilder.
SetSignalData
¶ Sets all signal data.
Signature
SetSignalData(signalData)
Parameters: signalData (list of NXOpen.Mechatronics.SignalAdapterBuilderSignalData_Struct
) – Array of signal dataNew in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
SignalAdapterBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.