RuntimeFormulaParameterBuilder Class¶
-
class
NXOpen.Mechatronics.
RuntimeFormulaParameterBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.RuntimeFormulaParameterBuilder
builderTo create a new instance of this class, use
NXOpen.Mechatronics.RuntimeFormulaCollection.CreateRuntimeFormulaParameterBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Alias | Returns or sets the Alias |
ParameterPhysics | Returns or sets the ParameterPhysics |
RuntimePropertyTag | Returns or sets the RuntimePropertyIndex |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Alias¶
-
RuntimeFormulaParameterBuilder.
Alias
¶ Returns or sets the Alias
-------------------------------------
Getter Method
Signature
Alias()
Returns: Return type: str New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Alias(name)
Parameters: name (str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ParameterPhysics¶
-
RuntimeFormulaParameterBuilder.
ParameterPhysics
¶ Returns or sets the ParameterPhysics
-------------------------------------
Getter Method
Signature
ParameterPhysics()
Returns: Return type: NXOpen.NXObject
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ParameterPhysics(praram)
Parameters: praram ( NXOpen.NXObject
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RuntimePropertyTag¶
-
RuntimeFormulaParameterBuilder.
RuntimePropertyTag
¶ Returns or sets the RuntimePropertyIndex
-------------------------------------
Getter Method
Signature
RuntimePropertyTag()
Returns: Return type: int New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
RuntimePropertyTag(tagProp)
Parameters: tagProp (int) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
RuntimeFormulaParameterBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.