PathConstraintJointCollection Class¶
-
class
NXOpen.Mechatronics.
PathConstraintJointCollection
¶ Bases:
object
Represents a collection of Path Constraint Joint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreatePathConstraintJointBuilder | Creates a NXOpen.Mechatronics.PathConstraintJointBuilder . |
FindObject | Finds the NXOpen.Mechatronics.PathConstraintJoint with the given name. |
Method Detail¶
CreatePathConstraintJointBuilder¶
-
PathConstraintJointCollection.
CreatePathConstraintJointBuilder
¶ Creates a
NXOpen.Mechatronics.PathConstraintJointBuilder
.Signature
CreatePathConstraintJointBuilder(slide)
Parameters: slide ( NXOpen.Mechatronics.PathConstraintJoint
) –NXOpen.Mechatronics.PathConstraintJoint
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.PathConstraintJointBuilder
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
PathConstraintJointCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.PathConstraintJoint
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.PathConstraintJoint
.Returns: NXOpen.Mechatronics.PathConstraintJoint
with this name.Return type: NXOpen.Mechatronics.PathConstraintJoint
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)