MotionProfileBuilder Class¶
-
class
NXOpen.Mechatronics.
MotionProfileBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.MotionProfile
builder.To create a new instance of this class, use
NXOpen.Mechatronics.MotionProfileCollection.CreateMotionProfileBuilder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
CyclicType | Returns or sets the cyclic type of a cam profile |
IsForElecCam | Returns or sets the indicator that a motion profile is designed for a electronic cam |
MasterMaximum | Returns the masterMax. |
MasterMinimum | Returns the masterMin. |
MasterUnit | Returns or sets the masterUnit. |
Name | Returns or sets the name |
SlaveMaximum | Returns the slaveMax. |
SlaveMinimum | Returns the slaveMin. |
SlaveUnit | Returns or sets the slaveUnit. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddElement | Add element to builder. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MotionProfileBuilderMasterValueUnit Enumeration | the Master Unit types |
MotionProfileBuilderProfileCyclicType Enumeration | Indicates which cyclic type should be take. |
MotionProfileBuilderSlaveValueUnit Enumeration | the Slave Unit types |
Property Detail¶
CyclicType¶
-
MotionProfileBuilder.
CyclicType
¶ Returns or sets the cyclic type of a cam profile
-------------------------------------
Getter Method
Signature
CyclicType()
Returns: Return type: NXOpen.Mechatronics.MotionProfileBuilderProfileCyclicType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CyclicType(cyclicType)
Parameters: cyclicType ( NXOpen.Mechatronics.MotionProfileBuilderProfileCyclicType
) –New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
IsForElecCam¶
-
MotionProfileBuilder.
IsForElecCam
¶ Returns or sets the indicator that a motion profile is designed for a electronic cam
-------------------------------------
Getter Method
Signature
IsForElecCam()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsForElecCam(isForElecCam)
Parameters: isForElecCam (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MasterMaximum¶
-
MotionProfileBuilder.
MasterMaximum
¶ Returns the masterMax.
-------------------------------------
Getter Method
Signature
MasterMaximum()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MasterMinimum¶
-
MotionProfileBuilder.
MasterMinimum
¶ Returns the masterMin.
-------------------------------------
Getter Method
Signature
MasterMinimum()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MasterUnit¶
-
MotionProfileBuilder.
MasterUnit
¶ Returns or sets the masterUnit.
-------------------------------------
Getter Method
Signature
MasterUnit()
Returns: Return type: NXOpen.Mechatronics.MotionProfileBuilderMasterValueUnit
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MasterUnit(masterUnit)
Parameters: masterUnit ( NXOpen.Mechatronics.MotionProfileBuilderMasterValueUnit
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Name¶
-
MotionProfileBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SlaveMaximum¶
-
MotionProfileBuilder.
SlaveMaximum
¶ Returns the slaveMax.
-------------------------------------
Getter Method
Signature
SlaveMaximum()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SlaveMinimum¶
-
MotionProfileBuilder.
SlaveMinimum
¶ Returns the slaveMin.
-------------------------------------
Getter Method
Signature
SlaveMinimum()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SlaveUnit¶
-
MotionProfileBuilder.
SlaveUnit
¶ Returns or sets the slaveUnit.
-------------------------------------
Getter Method
Signature
SlaveUnit()
Returns: Return type: NXOpen.Mechatronics.MotionProfileBuilderSlaveValueUnit
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
SlaveUnit(slaveUnit)
Parameters: slaveUnit ( NXOpen.Mechatronics.MotionProfileBuilderSlaveValueUnit
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
AddElement¶
-
MotionProfileBuilder.
AddElement
¶ Add element to builder.
Signature
AddElement(part, name, masterPos, slavePos, vin, vout, ain, aout, vinEqVout, ainEqAout, constantSpeed)
Parameters: - part (
NXOpen.NXObject
) – - name (str) –
- masterPos (float) –
- slavePos (float) –
- vin (float) –
- vout (float) –
- ain (float) –
- aout (float) –
- vinEqVout (bool) –
- ainEqAout (bool) –
- constantSpeed (bool) –
New in version NX8.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
- part (
Validate¶
-
MotionProfileBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.