LinearSpringJointCollection Class¶
-
class
NXOpen.Mechatronics.
LinearSpringJointCollection
¶ Bases:
object
Represents a collection of Linear Spring Joint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateLinearSpringJointBuilder | Creates a NXOpen.Mechatronics.LinearSpringJointBuilder . |
FindObject | Finds the NXOpen.Mechatronics.LinearSpringJoint with the given name. |
Method Detail¶
CreateLinearSpringJointBuilder¶
-
LinearSpringJointCollection.
CreateLinearSpringJointBuilder
¶ Creates a
NXOpen.Mechatronics.LinearSpringJointBuilder
.Signature
CreateLinearSpringJointBuilder(linearSpringJoint)
Parameters: linearSpringJoint ( NXOpen.Mechatronics.LinearSpringJoint
) –NXOpen.Mechatronics.LinearSpringJoint
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.LinearSpringJointBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
LinearSpringJointCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.LinearSpringJoint
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.LinearSpringJoint
.Returns: NXOpen.Mechatronics.LinearSpringJoint
with this name.Return type: NXOpen.Mechatronics.LinearSpringJoint
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)