GraphControlCollection Class¶
-
class
NXOpen.Mechatronics.
GraphControlCollection
¶ Bases:
object
Represents a collection of Graph Control.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CreateGraphControlBuilder | Creates a NXOpen.Mechatronics.GraphControlBuilder . |
FindObject | Finds the NXOpen.Mechatronics.GraphControl with the given name. |
Method Detail¶
CreateGraphControlBuilder¶
-
GraphControlCollection.
CreateGraphControlBuilder
¶ Creates a
NXOpen.Mechatronics.GraphControlBuilder
.Signature
CreateGraphControlBuilder(graphControl)
Parameters: graphControl ( NXOpen.Mechatronics.GraphControl
) –NXOpen.Mechatronics.GraphControl
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.GraphControlBuilder
New in version NX8.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
GraphControlCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.GraphControl
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.GraphControl
.Returns: NXOpen.Mechatronics.GraphControl
with this name.Return type: NXOpen.Mechatronics.GraphControl
New in version NX8.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)