GanttLinkerBuilder Class

class NXOpen.Mechatronics.GanttLinkerBuilder

Bases: NXOpen.Builder

Represents a NXOpen.Mechatronics.GanttLinkerBuilder

To create a new instance of this class, use NXOpen.Mechatronics.GanttLinkerCollection.CreateGanttLinkerBuilder

New in version NX10.0.0.

Properties

Property Description
Primary Returns or sets the accessor for first operation tag which is going to be linked
Secondary Returns or sets the accessor for second operation tag which is going to be linked
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

Primary

GanttLinkerBuilder.Primary

Returns or sets the accessor for first operation tag which is going to be linked

-------------------------------------

Getter Method

Signature Primary()

Returns:
Return type:NXOpen.Mechatronics.GanttOperationObject

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

-------------------------------------

Setter Method

Signature Primary(primary)

Parameters:primary (NXOpen.Mechatronics.GanttOperationObject) –

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

Secondary

GanttLinkerBuilder.Secondary

Returns or sets the accessor for second operation tag which is going to be linked

-------------------------------------

Getter Method

Signature Secondary()

Returns:
Return type:NXOpen.Mechatronics.GanttOperationObject

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

-------------------------------------

Setter Method

Signature Secondary(secondary)

Parameters:secondary (NXOpen.Mechatronics.GanttOperationObject) –

New in version NX10.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

Method Detail

Validate

GanttLinkerBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.