FunctionObjectBuilder Class¶
-
class
NXOpen.Mechatronics.
FunctionObjectBuilder
¶ Bases:
NXOpen.Mechatronics.SystemObjectBuilder
Represents a
NXOpen.Mechatronics.FunctionObjectBuilder
To create a new instance of this class, use
NXOpen.Mechatronics.FunctionObjectCollection.CreateFunctionObjectBuilder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
ExampleDesc | Returns or sets the example description |
FunctionItemRevisionId | Returns or sets the part id |
FunctionOptionSet | Returns or sets the option set |
InstanceName | Returns or sets the name of instance. |
LetterName | Returns or sets the letter name |
Modified | Returns or sets the modified status. |
NavigatorObject | Returns the navigator object which holds the teamcenter attributes. |
ObjectInformation | Returns the object information builder, used to specify the information of function object. |
ObjectName | Returns or sets the object name |
Parent | Returns or sets the parent |
PlmxmlFileName | Returns or sets the plmxml file name |
Tag | Returns the Tag for this object. |
TypeDesc | Returns or sets the type description |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetChildren | Gets the children |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOccurrences | Gets the occurrences |
GetOperations | Gets the operations |
GetParameterData | Gets the parameter data @return Parameter data array |
GetRequirementData | Gets the requirement data @return Requirement data array |
SetChildren | Sets the children |
SetOccurrences | Sets the occurrences |
SetOperations | Sets the operations |
SetParameterData | Sets the parameter data |
SetRequirementData | Sets the requirement data |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Structs¶
FunctionObjectBuilderParameterData_Struct Struct | Defined Parameter Data Structure |
FunctionObjectBuilderRequirementData_Struct Struct | Defined Requirement Data Structure |
Property Detail¶
ExampleDesc¶
-
FunctionObjectBuilder.
ExampleDesc
¶ Returns or sets the example description
-------------------------------------
Getter Method
Signature
ExampleDesc()
Returns: Example description Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ExampleDesc(exampleDesc)
Parameters: exampleDesc (str) – Example description New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FunctionItemRevisionId¶
-
FunctionObjectBuilder.
FunctionItemRevisionId
¶ Returns or sets the part id
-------------------------------------
Getter Method
Signature
FunctionItemRevisionId()
Returns: Function Revision Item id Return type: str New in version NX7.5.1.
Deprecated since version NX8.5.0: Please use
NXOpen.Mechatronics.ObjectInformationBuilder
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
FunctionItemRevisionId(functionItemId)
Parameters: functionItemId (str) – Function Revision Item id New in version NX7.5.1.
Deprecated since version NX8.5.0: Please use
NXOpen.Mechatronics.ObjectInformationBuilder
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FunctionOptionSet¶
-
FunctionObjectBuilder.
FunctionOptionSet
¶ Returns or sets the option set
-------------------------------------
Getter Method
Signature
FunctionOptionSet()
Returns: Function Option Set Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
FunctionOptionSet(functionOptionSet)
Parameters: functionOptionSet (str) – Function Option Set New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LetterName¶
-
FunctionObjectBuilder.
LetterName
¶ Returns or sets the letter name
-------------------------------------
Getter Method
Signature
LetterName()
Returns: Letter name Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
LetterName(letterName)
Parameters: letterName (str) – Letter name New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Modified¶
-
FunctionObjectBuilder.
Modified
¶ Returns or sets the modified status.
-------------------------------------
Getter Method
Signature
Modified()
Returns: Return type: bool New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Modified(modified)
Parameters: modified (bool) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ObjectInformation¶
-
FunctionObjectBuilder.
ObjectInformation
¶ Returns the object information builder, used to specify the information of function object.
-------------------------------------
Getter Method
Signature
ObjectInformation()
Returns: object information Builder Return type: NXOpen.Mechatronics.ObjectInformationBuilder
New in version NX8.5.0.
License requirements: None.
ObjectName¶
-
FunctionObjectBuilder.
ObjectName
¶ Returns or sets the object name
-------------------------------------
Getter Method
Signature
ObjectName()
Returns: Object name Return type: str New in version NX7.5.1.
Deprecated since version NX8.5.0: Please use
NXOpen.Mechatronics.ObjectInformationBuilder
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ObjectName(objectName)
Parameters: objectName (str) – Object name New in version NX7.5.1.
Deprecated since version NX8.5.0: Please use
NXOpen.Mechatronics.ObjectInformationBuilder
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Parent¶
-
FunctionObjectBuilder.
Parent
¶ Returns or sets the parent
-------------------------------------
Getter Method
Signature
Parent()
Returns: Parent function object Return type: NXOpen.NXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Parent(children)
Parameters: children ( NXOpen.NXObject
) – Parent function objectNew in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PlmxmlFileName¶
-
FunctionObjectBuilder.
PlmxmlFileName
¶ Returns or sets the plmxml file name
-------------------------------------
Getter Method
Signature
PlmxmlFileName()
Returns: PLMXML file name Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
PlmxmlFileName(plmxmlFileName)
Parameters: plmxmlFileName (str) – PLMXML file name New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
TypeDesc¶
-
FunctionObjectBuilder.
TypeDesc
¶ Returns or sets the type description
-------------------------------------
Getter Method
Signature
TypeDesc()
Returns: Type description Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
TypeDesc(typeDesc)
Parameters: typeDesc (str) – Type description New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetChildren¶
-
FunctionObjectBuilder.
GetChildren
¶ Gets the children
Signature
GetChildren()
Returns: Children object array Return type: list of NXOpen.NXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetOccurrences¶
-
FunctionObjectBuilder.
GetOccurrences
¶ Gets the occurrences
Signature
GetOccurrences()
Returns: Occurrences object array Return type: list of NXOpen.NXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetOperations¶
-
FunctionObjectBuilder.
GetOperations
¶ Gets the operations
Signature
GetOperations()
Returns: Operations object array Return type: list of NXOpen.NXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetParameterData¶
-
FunctionObjectBuilder.
GetParameterData
¶ Gets the parameter data
Signature
GetParameterData()
Returns: Parameter data array Return type: list of NXOpen.Mechatronics.FunctionObjectBuilderParameterData_Struct
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetRequirementData¶
-
FunctionObjectBuilder.
GetRequirementData
¶ Gets the requirement data
Signature
GetRequirementData()
Returns: Requirement data array Return type: list of NXOpen.Mechatronics.FunctionObjectBuilderRequirementData_Struct
New in version NX7.5.1.
Deprecated since version NX8.5.0: Please use
NXOpen.Mechatronics.RequirementBuilder
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetChildren¶
-
FunctionObjectBuilder.
SetChildren
¶ Sets the children
Signature
SetChildren(children)
Parameters: children (list of NXOpen.NXObject
) – Children object arrayNew in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetOccurrences¶
-
FunctionObjectBuilder.
SetOccurrences
¶ Sets the occurrences
Signature
SetOccurrences(occurrences)
Parameters: occurrences (list of NXOpen.NXObject
) – Occurrences object arrayNew in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetOperations¶
-
FunctionObjectBuilder.
SetOperations
¶ Sets the operations
Signature
SetOperations(operations)
Parameters: operations (list of NXOpen.NXObject
) – Operations object arrayNew in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetParameterData¶
-
FunctionObjectBuilder.
SetParameterData
¶ Sets the parameter data
Signature
SetParameterData(parameterData)
Parameters: parameterData (list of NXOpen.Mechatronics.FunctionObjectBuilderParameterData_Struct
) – Parameter data arrayNew in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetRequirementData¶
-
FunctionObjectBuilder.
SetRequirementData
¶ Sets the requirement data
Signature
SetRequirementData(requirementData)
Parameters: requirementData (list of NXOpen.Mechatronics.FunctionObjectBuilderRequirementData_Struct
) – Requirement data arrayNew in version NX7.5.1.
Deprecated since version NX8.5.0: Please use
NXOpen.Mechatronics.RequirementBuilder
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
FunctionObjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.