FixedJointCollection Class¶
-
class
NXOpen.Mechatronics.
FixedJointCollection
¶ Bases:
object
Represents a collection of Fixed Joint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateFixedJointBuilder | Creates a NXOpen.Mechatronics.FixedJointBuilder . |
FindObject | Finds the NXOpen.Mechatronics.FixedJoint with the given name. |
Method Detail¶
CreateFixedJointBuilder¶
-
FixedJointCollection.
CreateFixedJointBuilder
¶ Creates a
NXOpen.Mechatronics.FixedJointBuilder
.Signature
CreateFixedJointBuilder(slide)
Parameters: slide ( NXOpen.Mechatronics.FixedJoint
) –NXOpen.Mechatronics.FixedJoint
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.FixedJointBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
FixedJointCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.FixedJoint
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.FixedJoint
.Returns: NXOpen.Mechatronics.FixedJoint
with this name.Return type: NXOpen.Mechatronics.FixedJoint
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)