ECADImportBuilder Class¶
-
class
NXOpen.Mechatronics.
ECADImportBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ECADImportBuilder
To create a new instance of this class, use
NXOpen.Mechatronics.PhysicsManager.CreateECADImportBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ImportFile | Returns or sets the import file name |
PositionMethod | Returns or sets the position method, which is used in adding to assembly. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CompareObjects | Compares imported ECAD objects with logical objects. |
CreateLogicalNode | Creates logical node in system navigator. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditLogicalNode | Edits logical node in system navigator. |
GenerateEcadModelComponent | Generates ECAD model component. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ECADImportBuilderPositionMode Enumeration | Represents the position mode. |
Property Detail¶
ImportFile¶
-
ECADImportBuilder.
ImportFile
¶ Returns or sets the import file name
-------------------------------------
Getter Method
Signature
ImportFile()
Returns: The import file name Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImportFile(importFile)
Parameters: importFile (str) – The import file name New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PositionMethod¶
-
ECADImportBuilder.
PositionMethod
¶ Returns or sets the position method, which is used in adding to assembly.
-------------------------------------
Getter Method
Signature
PositionMethod()
Returns: Return type: NXOpen.Mechatronics.ECADImportBuilderPositionMode
New in version NX8.5.0.
Deprecated since version NX9.0.0: This method has no replacement. It is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
PositionMethod(positionMethod)
Parameters: positionMethod ( NXOpen.Mechatronics.ECADImportBuilderPositionMode
) –New in version NX8.5.0.
Deprecated since version NX9.0.0: This method has no replacement. It is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
CompareObjects¶
-
ECADImportBuilder.
CompareObjects
¶ Compares imported ECAD objects with logical objects.
Signature
CompareObjects()
Returns: The comparison result context Return type: NXOpen.Mechatronics.ComparisonResultContext
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CreateLogicalNode¶
-
ECADImportBuilder.
CreateLogicalNode
¶ Creates logical node in system navigator.
Signature
CreateLogicalNode(referenceDesignator)
Parameters: referenceDesignator (str) – Multiple Reference Designator Returns: Return type: NXOpen.Mechatronics.LogicObject
New in version NX8.5.0.
Deprecated since version NX9.0.0: This method has no replacement. It is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EditLogicalNode¶
-
ECADImportBuilder.
EditLogicalNode
¶ Edits logical node in system navigator.
Signature
EditLogicalNode(logicalNode, itemName, itemId, oldPartOcc, newPartOcc, parameterData)
Parameters: - logicalNode (
NXOpen.Mechatronics.LogicObject
) – - itemName (str) – Logical Item Name
- itemId (str) – Logical Item ID
- oldPartOcc (
NXOpen.Assemblies.Component
) – Old Component - newPartOcc (
NXOpen.Assemblies.Component
) – New Component - parameterData (list of
NXOpen.Mechatronics.LogicObjectBuilderParameterData_Struct
) – Parameter Data Array
New in version NX8.5.0.
Deprecated since version NX9.0.0: This method has no replacement. It is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
- logicalNode (
GenerateEcadModelComponent¶
-
ECADImportBuilder.
GenerateEcadModelComponent
¶ Generates ECAD model component.
Signature
GenerateEcadModelComponent(partName)
Parameters: partName (str) – ECAD Model Part Name NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: NXOpen.BasePart
New in version NX8.5.0.
Deprecated since version NX9.0.0: This method has no replacement. It is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ECADImportBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.