DisplayChangerCollection Class¶
-
class
NXOpen.Mechatronics.
DisplayChangerCollection
¶ Bases:
object
Represents a collection of Object Transformer.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateDisplayChangerBuilder | Creates a NXOpen.Mechatronics.DisplayChangerBuilder . |
FindObject | Finds the NXOpen.Mechatronics.DisplayChanger with the given name. |
Method Detail¶
CreateDisplayChangerBuilder¶
-
DisplayChangerCollection.
CreateDisplayChangerBuilder
¶ Creates a
NXOpen.Mechatronics.DisplayChangerBuilder
.Signature
CreateDisplayChangerBuilder(objectSrc)
Parameters: objectSrc ( NXOpen.Mechatronics.DisplayChanger
) –NXOpen.Mechatronics.DisplayChanger
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.DisplayChangerBuilder
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
DisplayChangerCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.DisplayChanger
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.DisplayChanger
.Returns: NXOpen.Mechatronics.DisplayChanger
with this name.Return type: NXOpen.Mechatronics.DisplayChanger
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)