CurveOnCurveJointBuilder Class¶
-
class
NXOpen.Mechatronics.
CurveOnCurveJointBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsJointBuilder
Represents a
NXOpen.Mechatronics.CurveOnCurveJoint
builderTo create a new instance of this class, use
NXOpen.Mechatronics.CurveOnCurveJointCollection.CreateCurveOnCurveJointBuilder
Default values.
Property Value Offset.Value 0 (millimeters part), 0 (inches part) Sliding 0 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Attachment | Returns the attachment of joint. |
AxisVector | Returns or sets the axis vector which is tangent to the connected curve at the selected point |
Base | Returns the base of joint. |
Name | Returns or sets the name. |
Offset | Returns the offset specifies the Zero Point on the curve whose distance to the point along the curve is the offset value. |
PointOnCurve | Returns or sets the selected point on curve |
Sliding | Returns or sets the sliding |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EvaluatePath | Evaluate the path. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetConnectedCurve | Get the connected curve which the attachment will move along @return curve or edge |
GetObject | Returns the object currently being edited by this builder. |
GetSectionCurve | Get the section curve which belong to the attachment @return curve or edge |
SetAttachment | Sets the attachment. |
SetBase | Sets the base. |
SetConnectedCurve | Set the connected curve which the attachment will move along |
SetSectionCurve | Set the section curve which belong to the attachment |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AxisVector¶
-
CurveOnCurveJointBuilder.
AxisVector
¶ Returns or sets the axis vector which is tangent to the connected curve at the selected point
-------------------------------------
Getter Method
Signature
AxisVector()
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AxisVector(axisVector)
Parameters: axisVector ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Offset¶
-
CurveOnCurveJointBuilder.
Offset
¶ Returns the offset specifies the “Zero Point” on the curve whose distance to the point along the curve is the offset value.
Zero Point is on the opposite direction of the axis with respect to the point on the curve.
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PointOnCurve¶
-
CurveOnCurveJointBuilder.
PointOnCurve
¶ Returns or sets the selected point on curve
-------------------------------------
Getter Method
Signature
PointOnCurve()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
PointOnCurve(pointOnCurve)
Parameters: pointOnCurve ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Sliding¶
-
CurveOnCurveJointBuilder.
Sliding
¶ Returns or sets the sliding
-------------------------------------
Getter Method
Signature
Sliding()
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Sliding(sliding)
Parameters: sliding (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
EvaluatePath¶
-
CurveOnCurveJointBuilder.
EvaluatePath
¶ Evaluate the path.
If there is no path, create it, otherwise evaluate it.
Signature
EvaluatePath(curves)
Parameters: curves (list of NXOpen.NXObject
) – curve or edgeNew in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetConnectedCurve¶
-
CurveOnCurveJointBuilder.
GetConnectedCurve
¶ Get the connected curve which the attachment will move along
Signature
GetConnectedCurve()
Returns: curve or edge Return type: list of NXOpen.NXObject
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetSectionCurve¶
-
CurveOnCurveJointBuilder.
GetSectionCurve
¶ Get the section curve which belong to the attachment
Signature
GetSectionCurve()
Returns: curve or edge Return type: list of NXOpen.NXObject
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetConnectedCurve¶
-
CurveOnCurveJointBuilder.
SetConnectedCurve
¶ Set the connected curve which the attachment will move along
Signature
SetConnectedCurve(curves)
Parameters: curves (list of NXOpen.NXObject
) – curve or edgeNew in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetSectionCurve¶
-
CurveOnCurveJointBuilder.
SetSectionCurve
¶ Set the section curve which belong to the attachment
Signature
SetSectionCurve(curves)
Parameters: curves (list of NXOpen.NXObject
) – curve or edgeNew in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
CurveOnCurveJointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.