ChangeOwnerBuilder Class¶
-
class
NXOpen.Mechatronics.
ChangeOwnerBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ChangeOwnerBuilder
.Which is able to move physics objects to a specific component. When
Builder.Commit
is called None will be returned.To create a new instance of this class, use
NXOpen.Mechatronics.PhysicsManager.CreateChangeOwnerBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Component | Returns the component which is expected to be the owner of physics objects. |
PhysicsObject | Returns the physics object. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CheckButton | Check the action is valid or not, and give the report in an information window. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Component¶
-
ChangeOwnerBuilder.
Component
¶ Returns the component which is expected to be the owner of physics objects.
-------------------------------------
Getter Method
Signature
Component()
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX10.0.0.
License requirements: None.
PhysicsObject¶
-
ChangeOwnerBuilder.
PhysicsObject
¶ Returns the physics object.
This can be
NXOpen.Mechatronics.RigidBody
,NXOpen.Mechatronics.PhysicsJoint
,NXOpen.Mechatronics.PhysicsConstraint
or other type of physics object.-------------------------------------
Getter Method
Signature
PhysicsObject()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX10.0.0.
License requirements: None.
Method Detail¶
CheckButton¶
-
ChangeOwnerBuilder.
CheckButton
¶ Check the action is valid or not, and give the report in an information window.
Signature
CheckButton()
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ChangeOwnerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.