AngularSpringJointCollection Class¶
-
class
NXOpen.Mechatronics.
AngularSpringJointCollection
¶ Bases:
object
Represents a collection of Angular Spring Joint.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
CreateAngularSpringJointBuilder | Creates a NXOpen.Mechatronics.AngularSpringJointBuilder . |
FindObject | Finds the NXOpen.Mechatronics.AngularSpringJoint with the given name. |
Method Detail¶
CreateAngularSpringJointBuilder¶
-
AngularSpringJointCollection.
CreateAngularSpringJointBuilder
¶ Creates a
NXOpen.Mechatronics.AngularSpringJointBuilder
.Signature
CreateAngularSpringJointBuilder(angularSpring)
Parameters: angularSpring ( NXOpen.Mechatronics.AngularSpringJoint
) –NXOpen.Mechatronics.AngularSpringJoint
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.AngularSpringJointBuilder
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
AngularSpringJointCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.AngularSpringJoint
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.AngularSpringJoint
.Returns: NXOpen.Mechatronics.AngularSpringJoint
with this name.Return type: NXOpen.Mechatronics.AngularSpringJoint
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)