MeasureManagerEndpointType Enumeration¶
NXOpen.MeasureManager.EndpointType is an alias for NXOpen.MeasureManagerEndpointType
-
class
NXOpen.
MeasureManagerEndpointType
¶ Bases:
object
Indicates the end point to be used when lines or linear edges are referenced in an angle between two objects
Enum Members
Enum Member Enum Member Description None default for other entity typesStartPoint EndPoint -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-