LoadOptionsUpdateSubsetOnLoad Enumeration¶
NXOpen.LoadOptions.UpdateSubsetOnLoad is an alias for NXOpen.LoadOptionsUpdateSubsetOnLoad
-
class
NXOpen.
LoadOptionsUpdateSubsetOnLoad
¶ Bases:
object
Options for specifying what type of subset updation to be carried out while loading
New in version NX8.5.0.
Enum Members
Enum Member Enum Member Description None replay recipeReplayRecipe do not update-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-