ListingWindow Class¶
-
class
NXOpen.
ListingWindow
¶ Bases:
object
Represents a ListingWindow.
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Device | Returns the device type for the window. |
IsOpen | Returns a flag indicating whether the listing window is open. |
Methods¶
Method | Description |
---|---|
Close | Closes the stream to the listing window. |
CloseWindow | Closes the listing window actually from the UI. |
Open | Opens the listing window. |
SelectDevice | Changes where the listing window output is sent. |
WriteFullline | Writes a full line to the listing window. |
WriteLine | Writes a line to the listing window. |
Enumerations¶
ListingWindowDeviceType Enumeration | Describes the type of listing window |
Property Detail¶
Device¶
-
ListingWindow.
Device
¶ Returns the device type for the window.
The device type indicates whether the output for the listing window is sent to the Information window, to a file, or to both
-------------------------------------
Getter Method
Signature
Device()
Returns: Return type: NXOpen.ListingWindowDeviceType
New in version NX3.0.0.
License requirements: None.
IsOpen¶
-
ListingWindow.
IsOpen
¶ Returns a flag indicating whether the listing window is open.
To open the window, use
NXOpen.Arc
.-------------------------------------
Getter Method
Signature
IsOpen()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
Method Detail¶
Close¶
-
ListingWindow.
Close
¶ Closes the stream to the listing window.
The window itself is not closed. If the listing window is a file, this will flush the buffer and close the file.
Signature
Close()
New in version NX3.0.0.
License requirements: None.
CloseWindow¶
-
ListingWindow.
CloseWindow
¶ Closes the listing window actually from the UI.
Signature
CloseWindow()
New in version NX6.0.0.
License requirements: None.
Open¶
-
ListingWindow.
Open
¶ Opens the listing window.
The listing window must be open before lines can be written to it
Signature
Open()
New in version NX3.0.0.
License requirements: None.
SelectDevice¶
-
ListingWindow.
SelectDevice
¶ Changes where the listing window output is sent.
The listing window output can be sent to the Information window of the Unigraphics session, to a file, or to both.
Note: file output is buffered. If file output is used, the buffer will not be flushed until the output device is changed again. E.g. <code> ListingWindow.SelectDevice(File, “log.txt”) ListingWindow.Open() ListingWindow.WriteLine(“output”) ListingWindow.Close() ‘ buffer is not flushed yet ListingWindow.SelectDevice(Window, “”) ‘ now the buffer is flushed </code>
Signature
SelectDevice(deviceType, fileName)
Parameters: - deviceType (
NXOpen.ListingWindowDeviceType
) – The type of device (file, Information window, or both) - fileName (str) – Name of the file. Used only if the device type is file. NOTE: The full Unicode character set is not supported for this parameter.
New in version NX3.0.0.
License requirements: None.
- deviceType (
WriteFullline¶
-
ListingWindow.
WriteFullline
¶ Writes a full line to the listing window.
The listing window must be open before you can write to it. If the listing window is a file, the output is buffered, so the output may not appear in the file until the buffer gets flushed. The buffer is flushed when the listing window gets closed. And number of characters displayed in one line has no limit which is different from
NXOpen.ListingWindow.WriteLine
If None is passed in this method will do nothing.
Signature
WriteFullline(msg)
Parameters: msg (str) – Line to write NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.5.0.
License requirements: None.
WriteLine¶
-
ListingWindow.
WriteLine
¶ Writes a line to the listing window.
The listing window must be open before you can write to it. If the listing window is a file, the output is buffered, so the output may not appear in the file until the buffer gets flushed. The buffer is flushed when the listing window gets closed. And the maximum number of characters displayed in one line is 132.
If None is passed in this method will do nothing.
Signature
WriteLine(msg)
Parameters: msg (str) – Line to write NOTE: The full Unicode character set is not supported for this parameter. New in version NX3.0.0.
License requirements: None.