LineWidthOption Enumeration¶
-
class
NXOpen.
LineWidthOption
¶ Bases:
object
the line width options.
This is used in conjunction with
NXOpen.LineWidthBuilder
Enum Members
NXOpen.LineWidthBuilder.Width
“- “Default”, ” Default width. The builder interprets this option as per its need. ” “NoChange”, ” Do not modify the width. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.