UINodeUtils Class¶
-
class
NXOpen.LineDesigner.
UINodeUtils
¶ Bases:
object
Represents a utils of line designer for journaling uinode methods
Use the static method in this class to obtain an instance.
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
CalculateAndSetNameOfAGAttr | Creates a DB factory Node |
Rename | To Rename partition |
Method Detail¶
CalculateAndSetNameOfAGAttr¶
-
UINodeUtils.
CalculateAndSetNameOfAGAttr
¶ Creates a DB factory Node
Signature
CalculateAndSetNameOfAGAttr(attributeGroup, subAGName, resourceName)
Parameters: - attributeGroup (
NXOpen.PDM.AttributeGroup
) – - subAGName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- resourceName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
- attributeGroup (
Rename¶
-
UINodeUtils.
Rename
¶ To Rename partition
Signature
Rename(objtg, newName)
Parameters: - objtg (
NXOpen.LineDesigner.ModelProductionUnit
) – - newName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
- objtg (