SingleElementConveyorBuilder Class¶
-
class
NXOpen.LineDesigner.
SingleElementConveyorBuilder
¶ Bases:
NXOpen.Builder
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateSingleElementConveyorBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FirstConveyingSurfaceCroner | Returns or sets the first croner point |
KfObject | Returns the kf object |
MovingDirection | Returns or sets the dir vector |
PointOnConveyingSurface | Returns or sets the point on surface |
Reversible | Returns or sets the add railing toggle |
SecondConveyingSurfaceCorner | Returns or sets the second corner point |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FirstConveyingSurfaceCroner¶
-
SingleElementConveyorBuilder.
FirstConveyingSurfaceCroner
¶ Returns or sets the first croner point
-------------------------------------
Getter Method
Signature
FirstConveyingSurfaceCroner()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
FirstConveyingSurfaceCroner(firstConveyingSurfaceCroner)
Parameters: firstConveyingSurfaceCroner ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
KfObject¶
-
SingleElementConveyorBuilder.
KfObject
¶ Returns the kf object
-------------------------------------
Getter Method
Signature
KfObject()
Returns: Return type: NXOpen.KFObject
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
MovingDirection¶
-
SingleElementConveyorBuilder.
MovingDirection
¶ Returns or sets the dir vector
-------------------------------------
Getter Method
Signature
MovingDirection()
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
MovingDirection(dirVector)
Parameters: dirVector ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
PointOnConveyingSurface¶
-
SingleElementConveyorBuilder.
PointOnConveyingSurface
¶ Returns or sets the point on surface
-------------------------------------
Getter Method
Signature
PointOnConveyingSurface()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
PointOnConveyingSurface(pointOnConveyingSurface)
Parameters: pointOnConveyingSurface ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Reversible¶
-
SingleElementConveyorBuilder.
Reversible
¶ Returns or sets the add railing toggle
-------------------------------------
Getter Method
Signature
Reversible()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
Reversible(reversible)
Parameters: reversible (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SecondConveyingSurfaceCorner¶
-
SingleElementConveyorBuilder.
SecondConveyingSurfaceCorner
¶ Returns or sets the second corner point
-------------------------------------
Getter Method
Signature
SecondConveyingSurfaceCorner()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SecondConveyingSurfaceCorner(secondConveyingSurfaceCorner)
Parameters: secondConveyingSurfaceCorner ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
SingleElementConveyorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.