RailingFeatureBuilder Class¶
-
class
NXOpen.LineDesigner.
RailingFeatureBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
LineDesigner.RailingFeature
Features.FeatureBuilder
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateRailingFeatureBuilder
Default values.
Property Value EnumPostCrossStyle IBeam EnumRailCrossStyle Rectangle EnumSpacingType CountandSpan IntegerCount 2 LinearDimBottomElevation.Value 0 (millimeters part), 0 (inches part) LinearDimPitchBy.Value 100 (millimeters part), 4 (inches part) LinearDimPostCrossDia.Value 37.5 (millimeters part), 1.5 (inches part) LinearDimPostCrossLength.Value 37.5 (millimeters part), 1.5 (inches part) LinearDimPostCrossTickness.Value 3.35 (millimeters part), 0.13 (inches part) LinearDimPostCrossWidth.Value 37.5 (millimeters part), 1.5 (inches part) LinearDimPostHeight.Value 1067 (millimeters part), 42 (inches part) LinearDimPostSpacing.Value 100 (millimeters part), 4 (inches part) LinearDimRailCrossDia.Value 37.5 (millimeters part), 1.5 (inches part) LinearDimRailCrossLength.Value 37.5 (millimeters part), 1.57 (inches part) LinearDimRailCrossWidth.Value 37.5 (millimeters part), 1.5 (inches part) OnPathDimSpanBy.Expression.Value 1067 (millimeters part), 42 (inches part) PostOffset PostOnCurve New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
EnumPostCrossStyle | Returns or sets the enum post cross style |
EnumRailCrossStyle | Returns or sets the enum rail cross style |
EnumSpacingType | Returns or sets the enum spacing type |
IntegerCount | Returns or sets the integer count |
LinearDimBottomElevation | Returns the linear dim bottom elevation |
LinearDimPitchBy | Returns the linear dim pitch by |
LinearDimPostCrossDia | Returns the linear dim post cross dia |
LinearDimPostCrossLength | Returns the linear dim post cross length |
LinearDimPostCrossTickness | Returns the linear dim post cross tickness |
LinearDimPostCrossWidth | Returns the linear dim post cross width |
LinearDimPostHeight | Returns the linear dim post height |
LinearDimPostSpacing | Returns the linear dim post spacing |
LinearDimRailCrossDia | Returns the linear dim rail cross dia |
LinearDimRailCrossLength | Returns the linear dim rail cross length |
LinearDimRailCrossWidth | Returns the linear dim rail cross width |
OnPathDimSpanBy | Returns the on path dim span by |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PostOffset | Returns or sets the post offset |
SelectionCurves | Returns the selection curves |
SelectionPostCrossSection | Returns the selection post cross section |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RailingFeatureBuilderPostOffsetType Enumeration | |
RailingFeatureBuilderRailCrossStyle Enumeration | |
RailingFeatureBuilderSelPostcrossStyle Enumeration | |
RailingFeatureBuilderSpaceType Enumeration |
Property Detail¶
EnumPostCrossStyle¶
-
RailingFeatureBuilder.
EnumPostCrossStyle
¶ Returns or sets the enum post cross style
-------------------------------------
Getter Method
Signature
EnumPostCrossStyle()
Returns: Return type: NXOpen.LineDesigner.RailingFeatureBuilderSelPostcrossStyle
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
EnumPostCrossStyle(enumPostCrossStyle)
Parameters: enumPostCrossStyle ( NXOpen.LineDesigner.RailingFeatureBuilderSelPostcrossStyle
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
EnumRailCrossStyle¶
-
RailingFeatureBuilder.
EnumRailCrossStyle
¶ Returns or sets the enum rail cross style
-------------------------------------
Getter Method
Signature
EnumRailCrossStyle()
Returns: Return type: NXOpen.LineDesigner.RailingFeatureBuilderRailCrossStyle
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
EnumRailCrossStyle(enumRailCrossStyle)
Parameters: enumRailCrossStyle ( NXOpen.LineDesigner.RailingFeatureBuilderRailCrossStyle
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
EnumSpacingType¶
-
RailingFeatureBuilder.
EnumSpacingType
¶ Returns or sets the enum spacing type
-------------------------------------
Getter Method
Signature
EnumSpacingType()
Returns: Return type: NXOpen.LineDesigner.RailingFeatureBuilderSpaceType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
EnumSpacingType(enumSpacingType)
Parameters: enumSpacingType ( NXOpen.LineDesigner.RailingFeatureBuilderSpaceType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
IntegerCount¶
-
RailingFeatureBuilder.
IntegerCount
¶ Returns or sets the integer count
-------------------------------------
Getter Method
Signature
IntegerCount()
Returns: Return type: int New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
IntegerCount(integerCount)
Parameters: integerCount (int) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimBottomElevation¶
-
RailingFeatureBuilder.
LinearDimBottomElevation
¶ Returns the linear dim bottom elevation
-------------------------------------
Getter Method
Signature
LinearDimBottomElevation()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimPitchBy¶
-
RailingFeatureBuilder.
LinearDimPitchBy
¶ Returns the linear dim pitch by
-------------------------------------
Getter Method
Signature
LinearDimPitchBy()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimPostCrossDia¶
-
RailingFeatureBuilder.
LinearDimPostCrossDia
¶ Returns the linear dim post cross dia
-------------------------------------
Getter Method
Signature
LinearDimPostCrossDia()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimPostCrossLength¶
-
RailingFeatureBuilder.
LinearDimPostCrossLength
¶ Returns the linear dim post cross length
-------------------------------------
Getter Method
Signature
LinearDimPostCrossLength()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimPostCrossTickness¶
-
RailingFeatureBuilder.
LinearDimPostCrossTickness
¶ Returns the linear dim post cross tickness
-------------------------------------
Getter Method
Signature
LinearDimPostCrossTickness()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimPostCrossWidth¶
-
RailingFeatureBuilder.
LinearDimPostCrossWidth
¶ Returns the linear dim post cross width
-------------------------------------
Getter Method
Signature
LinearDimPostCrossWidth()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimPostHeight¶
-
RailingFeatureBuilder.
LinearDimPostHeight
¶ Returns the linear dim post height
-------------------------------------
Getter Method
Signature
LinearDimPostHeight()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimPostSpacing¶
-
RailingFeatureBuilder.
LinearDimPostSpacing
¶ Returns the linear dim post spacing
-------------------------------------
Getter Method
Signature
LinearDimPostSpacing()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimRailCrossDia¶
-
RailingFeatureBuilder.
LinearDimRailCrossDia
¶ Returns the linear dim rail cross dia
-------------------------------------
Getter Method
Signature
LinearDimRailCrossDia()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimRailCrossLength¶
-
RailingFeatureBuilder.
LinearDimRailCrossLength
¶ Returns the linear dim rail cross length
-------------------------------------
Getter Method
Signature
LinearDimRailCrossLength()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimRailCrossWidth¶
-
RailingFeatureBuilder.
LinearDimRailCrossWidth
¶ Returns the linear dim rail cross width
-------------------------------------
Getter Method
Signature
LinearDimRailCrossWidth()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
OnPathDimSpanBy¶
-
RailingFeatureBuilder.
OnPathDimSpanBy
¶ Returns the on path dim span by
-------------------------------------
Getter Method
Signature
OnPathDimSpanBy()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
PostOffset¶
-
RailingFeatureBuilder.
PostOffset
¶ Returns or sets the post offset
-------------------------------------
Getter Method
Signature
PostOffset()
Returns: Return type: NXOpen.LineDesigner.RailingFeatureBuilderPostOffsetType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
PostOffset(postOffset)
Parameters: postOffset ( NXOpen.LineDesigner.RailingFeatureBuilderPostOffsetType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SelectionCurves¶
-
RailingFeatureBuilder.
SelectionCurves
¶ Returns the selection curves
-------------------------------------
Getter Method
Signature
SelectionCurves()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SelectionPostCrossSection¶
-
RailingFeatureBuilder.
SelectionPostCrossSection
¶ Returns the selection post cross section
-------------------------------------
Getter Method
Signature
SelectionPostCrossSection()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
RailingFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.