RailOpeningFeatureBuilder Class¶
-
class
NXOpen.LineDesigner.
RailOpeningFeatureBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.RailOpeningFeature
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateRailOpeningFeatureBuilder
Default values.
Property Value LinearDimElevation.Value 650 (millimeters part), 25.6 (inches part) LinearDimGateThickness.Value 37.5 (millimeters part), 1.5 (inches part) LinearDimOpeningWidth.Value 350 (millimeters part), 14 (inches part) OpeningAddGate 0 OpeningStyleEnum Left New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
LinearDimElevation | Returns the linear dim elevation |
LinearDimGateThickness | Returns the linear dim gate thickness |
LinearDimOpeningWidth | Returns the linear dim opening width |
OpeningAddGate | Returns or sets the opening add gate |
OpeningStyleEnum | Returns or sets the opening style enum |
ReverseDirection | Returns or sets the reverse direction |
SelectPoint | Returns or sets the select point |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDirVector | The dir vector @return |
GetObject | Returns the object currently being edited by this builder. |
SetDirVector | |
SetRailingFeature | |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
LinearDimElevation¶
-
RailOpeningFeatureBuilder.
LinearDimElevation
¶ Returns the linear dim elevation
-------------------------------------
Getter Method
Signature
LinearDimElevation()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimGateThickness¶
-
RailOpeningFeatureBuilder.
LinearDimGateThickness
¶ Returns the linear dim gate thickness
-------------------------------------
Getter Method
Signature
LinearDimGateThickness()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimOpeningWidth¶
-
RailOpeningFeatureBuilder.
LinearDimOpeningWidth
¶ Returns the linear dim opening width
-------------------------------------
Getter Method
Signature
LinearDimOpeningWidth()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
OpeningAddGate¶
-
RailOpeningFeatureBuilder.
OpeningAddGate
¶ Returns or sets the opening add gate
-------------------------------------
Getter Method
Signature
OpeningAddGate()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
OpeningAddGate(openingAddGate)
Parameters: openingAddGate (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
OpeningStyleEnum¶
-
RailOpeningFeatureBuilder.
OpeningStyleEnum
¶ Returns or sets the opening style enum
-------------------------------------
Getter Method
Signature
OpeningStyleEnum()
Returns: Return type: NXOpen.LineDesigner.RailOpeningFeatureBuilderGateOpeningStyle
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
OpeningStyleEnum(openingStyleEnum)
Parameters: openingStyleEnum ( NXOpen.LineDesigner.RailOpeningFeatureBuilderGateOpeningStyle
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ReverseDirection¶
-
RailOpeningFeatureBuilder.
ReverseDirection
¶ Returns or sets the reverse direction
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SelectPoint¶
-
RailOpeningFeatureBuilder.
SelectPoint
¶ Returns or sets the select point
-------------------------------------
Getter Method
Signature
SelectPoint()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SelectPoint(selectPoint)
Parameters: selectPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
GetDirVector¶
-
RailOpeningFeatureBuilder.
GetDirVector
¶ The dir vector
Signature
GetDirVector()
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetDirVector¶
-
RailOpeningFeatureBuilder.
SetDirVector
¶ Signature
SetDirVector(dirVector)
Parameters: dirVector ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetRailingFeature¶
-
RailOpeningFeatureBuilder.
SetRailingFeature
¶ Signature
SetRailingFeature(railingFrec)
Parameters: railingFrec ( NXOpen.Features.Feature
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
RailOpeningFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.