InsertSheetBuilder Class¶
-
class
NXOpen.LineDesigner.
InsertSheetBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.InsertSheet
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateInsertSheetBuilder
Default values.
Property Value UnitsEnum Millimeters New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
NameString | Returns or sets the name string |
NumberString | Returns or sets the number string |
RevisionString | Returns or sets the revision string |
ScaleEnum | Returns or sets the scale enum |
SecondaryNumberString | Returns or sets the secondary number string |
SizeEnum | Returns or sets the size enum |
Tag | Returns the Tag for this object. |
UnitsEnum | Returns or sets the units enum |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InsertSheetBuilderAPIUnits Enumeration | Represents the units types |
Property Detail¶
NameString¶
-
InsertSheetBuilder.
NameString
¶ Returns or sets the name string
-------------------------------------
Getter Method
Signature
NameString()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
NameString(nameString)
Parameters: nameString (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
NumberString¶
-
InsertSheetBuilder.
NumberString
¶ Returns or sets the number string
-------------------------------------
Getter Method
Signature
NumberString()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
NumberString(numberString)
Parameters: numberString (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
RevisionString¶
-
InsertSheetBuilder.
RevisionString
¶ Returns or sets the revision string
-------------------------------------
Getter Method
Signature
RevisionString()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
RevisionString(revisionString)
Parameters: revisionString (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ScaleEnum¶
-
InsertSheetBuilder.
ScaleEnum
¶ Returns or sets the scale enum
-------------------------------------
Getter Method
Signature
ScaleEnum()
Returns: Return type: int New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ScaleEnum(scaleEnum)
Parameters: scaleEnum (int) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SecondaryNumberString¶
-
InsertSheetBuilder.
SecondaryNumberString
¶ Returns or sets the secondary number string
-------------------------------------
Getter Method
Signature
SecondaryNumberString()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SecondaryNumberString(secondaryNumberString)
Parameters: secondaryNumberString (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SizeEnum¶
-
InsertSheetBuilder.
SizeEnum
¶ Returns or sets the size enum
-------------------------------------
Getter Method
Signature
SizeEnum()
Returns: Return type: int New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SizeEnum(sizeEnum)
Parameters: sizeEnum (int) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UnitsEnum¶
-
InsertSheetBuilder.
UnitsEnum
¶ Returns or sets the units enum
-------------------------------------
Getter Method
Signature
UnitsEnum()
Returns: Return type: NXOpen.LineDesigner.InsertSheetBuilderAPIUnits
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
UnitsEnum(unitsEnum)
Parameters: unitsEnum ( NXOpen.LineDesigner.InsertSheetBuilderAPIUnits
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
InsertSheetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.