GlobalSelectionBuilder Class¶
-
class
NXOpen.LineDesigner.
GlobalSelectionBuilder
¶ Bases:
NXOpen.Builder
Global Selection
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateGlobalSelectionBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Selection | Returns the selected objects |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
BeginDrag | Begin Drag |
CleanupComponent | Cleanup |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDraggedObject | Get the dragged object @return |
GetObject | Returns the object currently being edited by this builder. |
MoveComponent | Move component |
OnDrag | On Drag |
ResetComponent | Reset component |
SetDraggedObject | Set the dragged object |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateAfterCleanup | UpdateAfterCleanUp |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Selection¶
-
GlobalSelectionBuilder.
Selection
¶ Returns the selected objects
-------------------------------------
Getter Method
Signature
Selection()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
BeginDrag¶
-
GlobalSelectionBuilder.
BeginDrag
¶ Begin Drag
Signature
BeginDrag()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
CleanupComponent¶
-
GlobalSelectionBuilder.
CleanupComponent
¶ Cleanup
Signature
CleanupComponent()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
GetDraggedObject¶
-
GlobalSelectionBuilder.
GetDraggedObject
¶ Get the dragged object
Signature
GetDraggedObject()
Returns: Return type: NXOpen.NXObject
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
MoveComponent¶
-
GlobalSelectionBuilder.
MoveComponent
¶ Move component
Signature
MoveComponent(translation)
Parameters: translation ( NXOpen.Vector3d
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
OnDrag¶
-
GlobalSelectionBuilder.
OnDrag
¶ On Drag
Signature
OnDrag(translation)
Parameters: translation ( NXOpen.Vector3d
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ResetComponent¶
-
GlobalSelectionBuilder.
ResetComponent
¶ Reset component
Signature
ResetComponent()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetDraggedObject¶
-
GlobalSelectionBuilder.
SetDraggedObject
¶ Set the dragged object
Signature
SetDraggedObject(draggedObject)
Parameters: draggedObject ( NXOpen.NXObject
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UpdateAfterCleanup¶
-
GlobalSelectionBuilder.
UpdateAfterCleanup
¶ UpdateAfterCleanUp
Signature
UpdateAfterCleanup()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
GlobalSelectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.