ExportPlantToDWGBuilder Class¶
-
class
NXOpen.LineDesigner.
ExportPlantToDWGBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.ExportPlantToDWG
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateExportPlantToDwgBuilder
Default values.
Property Value SaveAs T2d New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FileName | Returns or sets the file name |
FolderName | Returns or sets the folder name |
SaveAs | Returns or sets the save as |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExportPlantToDWGBuilderSaveAsType Enumeration | Represents the dwg saving types |
Property Detail¶
FileName¶
-
ExportPlantToDWGBuilder.
FileName
¶ Returns or sets the file name
-------------------------------------
Getter Method
Signature
FileName()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
FileName(fileName)
Parameters: fileName (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
FolderName¶
-
ExportPlantToDWGBuilder.
FolderName
¶ Returns or sets the folder name
-------------------------------------
Getter Method
Signature
FolderName()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
FolderName(foldername)
Parameters: foldername (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SaveAs¶
-
ExportPlantToDWGBuilder.
SaveAs
¶ Returns or sets the save as
-------------------------------------
Getter Method
Signature
SaveAs()
Returns: Return type: NXOpen.LineDesigner.ExportPlantToDWGBuilderSaveAsType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SaveAs(saveAs)
Parameters: saveAs ( NXOpen.LineDesigner.ExportPlantToDWGBuilderSaveAsType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
ExportPlantToDWGBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.